81 #ifndef DSPLIB_QRD_IXX_IXX_OXX_H_
82 #define DSPLIB_QRD_IXX_IXX_OXX_H_
84 #include "../common/DSPLIB_types.h"
214 const void *restrict pA,
215 const void *restrict pQ,
216 const void *restrict pR,
217 const void *restrict pU,
218 const void *restrict pScratch);
261 const void *restrict pA,
262 const void *restrict pQ,
263 const void *restrict pR,
264 const void *restrict pU,
265 const void *restrict pScratch);
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
DSPLIB_STATUS DSPLIB_qrd_init_checkParams(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsU, const DSPLIB_qrdInitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_qrd_init function....
int32_t DSPLIB_qrd_getHandleSize(DSPLIB_qrdInitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_qrd_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsU, const DSPLIB_qrdInitArgs *pKerInitArgs)
This function should be called before the DSPLIB_qrd_exec function is called. This function takes car...
DSPLIB_STATUS DSPLIB_qrd_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pQ, const void *restrict pR, const void *restrict pU, const void *restrict pScratch)
This function checks the validity of the parameters passed to DSPLIB_qrd_exec function....
DSPLIB_STATUS DSPLIB_qrd_exec(DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pQ, const void *restrict pR, const void *restrict pU, const void *restrict pScratch)
This function is the main kernel compute function.
A structure for a 1 dimensional buffer descriptor.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
uint32_t dimY
Size of input data.
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
uint32_t dimX
Size of input data.