![]() |
DSPLIB User Guide
|
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_negate.
Definition in file DSPLIB_negate_priv.h.
Go to the source code of this file.
Data Structures | |
| struct | DSPLIB_negate_PrivArgs |
| Structure that is reserved for internal use by the kernel. More... | |
Macros | |
| #define | SE_PARAM_BASE (0x0000) |
| #define | SE_SE0_PARAM_OFFSET (SE_PARAM_BASE) |
| #define | SE_SA0_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | DSPLIB_NEGATE_IXX_IXX_OXX_PBLOCK_SIZE (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t)) |
| Macro to define the size of bufPblock array of DSPLIB_negate_PrivArgs structure. More... | |
Typedefs | |
| typedef DSPLIB_STATUS(* | pFxnDSPLIB_negate_exec) (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This is a function pointer type that conforms to the declaration of DSPLIB_negate_exec_ci and DSPLIB_negate_exec_cn. More... | |
Functions | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_negate_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_negate_InitArgs *pKerInitArgs) |
| This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_negate_init. More... | |
| template<typename dataType , int32_t dataIn> | |
| DSPLIB_STATUS | DSPLIB_negate_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_negate_exec. More... | |
| template<typename dataType , int32_t dataIn> | |
| DSPLIB_STATUS | DSPLIB_negate_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_negate_exec. More... | |
| DSPLIB_STATUS | DSPLIB_negate_init_cn (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut) |
| This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_negate_init. More... | |
| #define SE_PARAM_BASE (0x0000) |
Definition at line 38 of file DSPLIB_negate_priv.h.
| #define SE_SE0_PARAM_OFFSET (SE_PARAM_BASE) |
Definition at line 39 of file DSPLIB_negate_priv.h.
| #define SE_SA0_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 40 of file DSPLIB_negate_priv.h.
| #define DSPLIB_NEGATE_IXX_IXX_OXX_PBLOCK_SIZE (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t)) |
Macro to define the size of bufPblock array of DSPLIB_negate_PrivArgs structure.
Definition at line 46 of file DSPLIB_negate_priv.h.
| typedef DSPLIB_STATUS(* pFxnDSPLIB_negate_exec) (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
This is a function pointer type that conforms to the declaration of DSPLIB_negate_exec_ci and DSPLIB_negate_exec_cn.
Definition at line 52 of file DSPLIB_negate_priv.h.
| DSPLIB_STATUS DSPLIB_negate_init_ci | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_negate_InitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_negate_init.
This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_negate_exec_ci would be called later independently by the application. When DSPLIB_negate_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_negate_exec_ci does not lose cycles to determine the hardware configuration.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 49 of file DSPLIB_negate_ci.cpp.
| DSPLIB_STATUS DSPLIB_negate_exec_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_negate_exec.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 120 of file DSPLIB_negate_ci.cpp.
| DSPLIB_STATUS DSPLIB_negate_exec_cn | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_negate_exec.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 33 of file DSPLIB_negate_cn.cpp.
| DSPLIB_STATUS DSPLIB_negate_init_cn | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams2D_t * | bufParamsIn, | ||
| DSPLIB_bufParams2D_t * | bufParamsOut | ||
| ) |
This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_negate_init.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |