31 template <
typename dataType>
38 uint32_t blockSize = pKerPrivArgs->
blockSize;
41 printf(
"Enter DSPLIB_mul_exec_cn\n");
44 dataType *pInLocal1 = (dataType *) pIn1;
45 dataType *pInLocal2 = (dataType *) pIn2;
46 dataType *pOutLocal = (dataType *) pOut;
49 printf(
"Enter pInLocal1 %p pInLocal2 %p pOut %p\n", pInLocal1, pInLocal2, pOut);
54 for (int32_t counter = 0; counter < blockSize; counter++) {
59 printf(
"counter %d a %d b %d\n", counter, a, b);
65 printf(
"counter %d y %d\n", counter, out);
template DSPLIB_STATUS DSPLIB_mul_exec_cn< uint16_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mul_exec_cn< uint8_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mul_exec_cn< int32_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
DSPLIB_STATUS DSPLIB_mul_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This function is the main execution function for the natural C implementation of the kernel....
template DSPLIB_STATUS DSPLIB_mul_exec_cn< double >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mul_exec_cn< int16_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mul_exec_cn< int8_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mul_exec_cn< float >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mul_exec_cn< uint32_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_mul.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
Structure that is reserved for internal use by the kernel.
int32_t blockSize
Size of input buffer for different batches DSPLIB_mul_init that will be retrieved and used by DSPLIB_...