Go to the source code of this file.
|
| template<typename dataType , int32_t dataIn> |
| DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| | This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_mulConstant_exec. More...
|
| |
| template DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn< float, DSPLIB_FLOAT32 > (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn< double, DSPLIB_FLOAT64 > (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn< int8_t, DSPLIB_INT8 > (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn< uint8_t, DSPLIB_UINT8 > (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn< int16_t, DSPLIB_INT16 > (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn< uint16_t, DSPLIB_UINT16 > (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn< int32_t, DSPLIB_INT32 > (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_mulConstant_exec_cn< uint32_t, DSPLIB_UINT32 > (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| |
◆ DSPLIB_mulConstant_exec_cn()
template<typename dataType , int32_t dataIn>
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_mulConstant_exec.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [in] | pFilterCoeff | Pointer to buffer holding the filter coefficient data |
| [in] | pFilterVar | : Pointer to buffer holding the filter variable data |
| [out] | pOut | : Pointer to buffer holding the output data |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 33 of file DSPLIB_mulConstant_cn.cpp.
◆ DSPLIB_mulConstant_exec_cn< float, DSPLIB_FLOAT32 >()
◆ DSPLIB_mulConstant_exec_cn< double, DSPLIB_FLOAT64 >()
◆ DSPLIB_mulConstant_exec_cn< int8_t, DSPLIB_INT8 >()
◆ DSPLIB_mulConstant_exec_cn< uint8_t, DSPLIB_UINT8 >()
◆ DSPLIB_mulConstant_exec_cn< int16_t, DSPLIB_INT16 >()
◆ DSPLIB_mulConstant_exec_cn< uint16_t, DSPLIB_UINT16 >()
◆ DSPLIB_mulConstant_exec_cn< int32_t, DSPLIB_INT32 >()
◆ DSPLIB_mulConstant_exec_cn< uint32_t, DSPLIB_UINT32 >()