DSPLIB User Guide
DSPLIB_maxIndex.cpp File Reference

Go to the source code of this file.

Functions

int32_t DSPLIB_maxIndex_getHandleSize (DSPLIB_maxIndex_InitArgs *pKerInitArgs)
 This is a query function to calculate the size of internal handle. More...
 
DSPLIB_STATUS DSPLIB_maxIndex_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_maxIndex_InitArgs *pKerInitArgs)
 This function checks the validity of the parameters passed to DSPLIB_maxIndex_init function. This function is called with the same parameters as the DSPLIB_maxIndex_init, and this function must be called before the DSPLIB_maxIndex_init is called. More...
 
DSPLIB_STATUS DSPLIB_maxIndex_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
 This function checks the validity of the parameters passed to DSPLIB_maxIndex_exec function. This function is called with the same parameters as the DSPLIB_maxIndex_init, and this function must be called before the DSPLIB_maxIndex_init is called. More...
 
DSPLIB_STATUS DSPLIB_maxIndex_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_maxIndex_InitArgs *pKerInitArgs)
 This function should be called before the DSPLIB_maxIndex_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More...
 
DSPLIB_STATUS DSPLIB_maxIndex_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This function is the main kernel compute function. More...