81 #ifndef DSPLIB_CHOLESKY_SOLVER_IXX_IXX_OXX_H_
82 #define DSPLIB_CHOLESKY_SOLVER_IXX_IXX_OXX_H_
85 #include "../common/DSPLIB_types.h"
227 const void *restrict pU,
228 const void *restrict pScratch,
229 const void *restrict pY,
230 const void *restrict pB,
231 const void *restrict pX,
232 const void *restrict pDiv);
275 void *restrict pScratch,
279 void *restrict pDiv);
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
DSPLIB_STATUS DSPLIB_cholesky_solver_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsU, DSPLIB_bufParams2D_t *bufParamsScratch, DSPLIB_bufParams1D_t *bufParamsY, DSPLIB_bufParams1D_t *bufParamsB, DSPLIB_bufParams1D_t *bufParamsX, DSPLIB_bufParams1D_t *bufParamsDiv, const DSPLIB_cholesky_solver_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_cholesky_solver_exec function is called....
DSPLIB_STATUS DSPLIB_cholesky_solver_exec(DSPLIB_kernelHandle handle, void *restrict pU, void *restrict pScratch, void *restrict pY, void *restrict pB, void *restrict pX, void *restrict pDiv)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_cholesky_solver_init_checkParams(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsU, DSPLIB_bufParams2D_t *bufParamsScratch, DSPLIB_bufParams1D_t *bufParamsY, DSPLIB_bufParams1D_t *bufParamsB, DSPLIB_bufParams1D_t *bufParamsX, DSPLIB_bufParams1D_t *bufParamsDiv, const DSPLIB_cholesky_solver_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_cholesky_solver_init function....
DSPLIB_STATUS DSPLIB_cholesky_solver_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pU, const void *restrict pScratch, const void *restrict pY, const void *restrict pB, const void *restrict pX, const void *restrict pDiv)
This function checks the validity of the parameters passed to DSPLIB_cholesky_solver_exec function....
int32_t DSPLIB_cholesky_solver_getHandleSize(DSPLIB_cholesky_solver_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
A structure for a 1 dimensional buffer descriptor.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
int32_t stride
stride of input/output data in ci
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
int32_t strideCn
stride of input/output data in cn
int32_t order
order of input data