81 #ifndef DSPLIB_CHOLESKY_INPLACE_IXX_IXX_OXX_H_
82 #define DSPLIB_CHOLESKY_INPLACE_IXX_IXX_OXX_H_
85 #include "../common/DSPLIB_types.h"
199 const void *restrict pA,
200 const void *restrict pMul);
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
int32_t DSPLIB_cholesky_inplace_getHandleSize(DSPLIB_cholesky_inplace_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_cholesky_inplace_init_checkParams(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams1D_t *bufParamsMul, const DSPLIB_cholesky_inplace_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_cholesky_inplace_init function....
DSPLIB_STATUS DSPLIB_cholesky_inplace_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams1D_t *bufParamsMul, const DSPLIB_cholesky_inplace_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_cholesky_inplace_exec function is called....
DSPLIB_STATUS DSPLIB_cholesky_inplace_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pMul)
This function checks the validity of the parameters passed to DSPLIB_cholesky_inplace_exec function....
DSPLIB_STATUS DSPLIB_cholesky_inplace_exec(DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pMul)
This function is the main kernel compute function.
A structure for a 1 dimensional buffer descriptor.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
int32_t stride
stride of input/output data in ci
int32_t order
order of input data
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
int32_t enableTest
flag to check for positive definiteness of input matrix