DSPLIB User Guide
DSPLIB_bexp_cn.cpp File Reference

Go to the source code of this file.

Functions

template<typename dataType >
DSPLIB_STATUS DSPLIB_bexp_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_exec. More...
 
template DSPLIB_STATUS DSPLIB_bexp_exec_cn< int8_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_bexp_exec_cn< uint8_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_bexp_exec_cn< int16_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_bexp_exec_cn< uint16_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_bexp_exec_cn< int32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_bexp_exec_cn< uint32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_bexp_exec_cn< int64_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_bexp_exec_cn< uint64_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 

Function Documentation

◆ DSPLIB_bexp_exec_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_bexp_exec_cn ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_exec.

C Natural implementation of the bexp kernels. Handles unsigned and signed data types internally

Definition at line 36 of file DSPLIB_bexp_cn.cpp.

◆ DSPLIB_bexp_exec_cn< int8_t >()

template DSPLIB_STATUS DSPLIB_bexp_exec_cn< int8_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_bexp_exec_cn< uint8_t >()

template DSPLIB_STATUS DSPLIB_bexp_exec_cn< uint8_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_bexp_exec_cn< int16_t >()

template DSPLIB_STATUS DSPLIB_bexp_exec_cn< int16_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_bexp_exec_cn< uint16_t >()

template DSPLIB_STATUS DSPLIB_bexp_exec_cn< uint16_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_bexp_exec_cn< int32_t >()

template DSPLIB_STATUS DSPLIB_bexp_exec_cn< int32_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_bexp_exec_cn< uint32_t >()

template DSPLIB_STATUS DSPLIB_bexp_exec_cn< uint32_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_bexp_exec_cn< int64_t >()

template DSPLIB_STATUS DSPLIB_bexp_exec_cn< int64_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_bexp_exec_cn< uint64_t >()

template DSPLIB_STATUS DSPLIB_bexp_exec_cn< uint64_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)