UDMA event object. More...
#include <udma_event.h>
Data Fields | |
| Udma_DrvHandle | drvHandle |
| Udma_EventPrms | eventPrms |
| uint32_t | globalEvent |
| uint32_t | vintrNum |
| uint32_t | vintrBitNum |
| uint32_t | irIntrNum |
| uint32_t | coreIntrNum |
| Udma_EventHandle | nextEvent |
| Udma_EventHandle | prevEvent |
| HwiP_Handle | hwiHandle |
| uint64_t | vintrBitAllocFlag |
| volatile CSL_intaggr_imapRegs_gevi * | pIaGeviRegs |
| volatile CSL_intaggr_intrRegs_vint * | pIaVintrRegs |
| uint32_t | eventInitDone |
UDMA event object.
UDMA event handle.
Note: This is an internal/private driver structure and should not be used or modified by caller.