OS Abstraction Layer header. More...
#include <ti/csl/tistdtypes.h>#include <ti/osal/TaskP.h>#include <ti/osal/HwiP.h>#include <ti/osal/MuxIntcP.h>#include <ti/osal/SemaphoreP.h>#include <ti/osal/CacheP.h>#include <ti/osal/TimerP.h>#include <ti/osal/RegisterIntr.h>#include <ti/osal/QueueP.h>#include <ti/osal/CycleprofilerP.h>#include <ti/osal/MailboxP.h>#include <ti/osal/MutexP.h>#include <ti/osal/ClockP.h>#include <ti/osal/DebugP.h>#include <ti/osal/HeapP.h>#include <ti/osal/MemoryP.h>#include <ti/osal/EventP.h>#include <ti/osal/StartuphooksP.h>Go to the source code of this file.
Data Structures | |
| struct | Osal_StaticMemStatus |
| This structure holds static memory status parameters of OSAL library. More... | |
| struct | Osal_memRange |
| Osal memory address range. More... | |
| struct | Osal_HwAttrs |
| Osal hw attributes structure. More... | |
Osal Error return Codes | |
| #define | osal_OK ((int32_t)(0)) |
| #define | osal_FAILURE (-(int32_t)(1)) |
| #define | osal_UNSUPPORTED (-(int32_t)(2)) |
| #define | osal_NOMEM (-(int32_t)(3)) |
| #define | osal_WAIT_FOREVER (~((uint32_t)0U)) |
| #define | osal_NO_WAIT ((uint32_t)0U) |
| #define | OSAL_NONOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 48U) |
| #define | OSAL_NONOS_HWIP_SIZE_BYTES ((uint32_t) 48U) |
| #define | OSAL_FREERTOS_HWIP_C7X_SIZE_BYTES ((uint32_t) 56U) |
| #define | OSAL_SAFERTOS_HWIP_C7X_SIZE_BYTES ((uint32_t) 56U) |
| #define | OSAL_FREERTOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 96U) |
| #define | OSAL_FREERTOS_TASKP_SIZE_BYTES ((uint32_t) 128U) |
| #define | OSAL_SAFERTOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 248U) |
| #define | OSAL_SAFERTOS_TASKP_SIZE_BYTES ((uint32_t) 248U) |
| #define | OSAL_Assert(expression) |
| Assert checking function. More... | |
| enum | Osal_ThreadType { Osal_ThreadType_Hwi , Osal_ThreadType_Swi , Osal_ThreadType_Task , Osal_ThreadType_Main , Osal_ThreadType_Abort } |
| This enum defines the multiple thread types used under OSAL library. More... | |
| enum | Osal_HwAccessType { OSAL_HWACCESS_UNRESTRICTED , OSAL_HWACCESS_RESTRICTED } |
| Osal hw access type. More... | |
| void | Osal_DebugP_assert (int32_t expression, const char *filename, int32_t line) |
| Osal_ThreadType | Osal_getThreadType (void) |
| Function to get the current thread type. More... | |
| int32_t | Osal_delay (uint32_t nTicks) |
| Function to delay/sleep the specified number of ticks. More... | |
Osal HwAttrs ValidBit definitions | |
| #define | OSAL_HWATTR_SET_EXT_CLK (0x00000001U) |
| #define | OSAL_HWATTR_SET_ECM_INT (0x00000002U) |
| #define | OSAL_HWATTR_SET_HWACCESS_TYPE (0x00000004U) |
| #define | OSAL_HWATTR_SET_OSALDELAY_TIMER_BASE (0x00000008U) |
| #define | OSAL_HWATTR_SET_SEMP_EXT_BASE (0x00000010U) |
| #define | OSAL_HWATTR_SET_HWIP_EXT_BASE (0x00000020U) |
| #define | OSAL_HWATTR_SET_CPU_FREQ (0x00000040U) |
| #define | OSAL_HWATTR_SET_TARG_PROC_LIST (0x00000080U) |
| #define | OSAL_COMPILE_TIME_SIZE_CHECK(x, y) |
| Osal_HwAttrs | gOsal_HwAttrs |
| external references for Osal Hw Attribute structure More... | |
| int32_t | Osal_setHwAttrs (uint32_t ctrlBitMap, const Osal_HwAttrs *hwAttrs) |
| Function to set the Hw Attributes. More... | |
| int32_t | Osal_getHwAttrs (Osal_HwAttrs *hwAttrs) |
| Function to get the Hw Attributes. More... | |
| int32_t | Osal_getStaticMemStatus (Osal_StaticMemStatus *pMemStat) |
| Function to get the static memory usage of OSAL library. More... | |
| uint32_t | Osal_getCoreId (void) |
| Function to get the core ID of the running Core. More... | |
| int32_t | Osal_isInPrivilegeMode (void) |
| Function to check if the calling task is in privileged mode. More... | |
| void | OS_init (void) |
| Function for initializing the OS / scheduler. More... | |
| void | OS_start (void) |
| Function to strat OS / scheduler. More... | |
| void | OS_stop (void) |
| Function to stop OS / scheduler. More... | |
OS Abstraction Layer header.
============================================================================