Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.
Processor SDK Linux Automotive Release Notes
Last updated: 12/16/2019
Contents
Overview
The Processor Software Development Kit (Processor-SDK) for Linux Automotive provides a foundation software platform for development, deployment and execution of Linux based applications for DRA7xx SoCs and includes the following:
- Bootloader, Linux Kernel & Filesystem
- SDK Installer
- Setup Scripts
- Makefiles
- Matrix Application Launcher
- Example Applications
Licensing
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor_SDK_Linux_GPLv3_Disclaimer
Documentation
- Software Developer's Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux Automotive release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Software Manifest: Provides license information on software included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application This document is provided as part of the EVM kit.
Release 06.00.00
Released in Dec 2019
What's New
Texas Instruments (TI) 's strategy is to upstream and align with the latest announced LTS Linux Kernel every year. All the code changes made by TI (both new features and bug fixes) are in their respective upstream or publicly available repositories. Linux Kernel v4.19 is the official LTS kernel for 2019.
This is the first Processor SDK Linux Automotive release on K4.19 supporting DRA7xx family of devices.
Features
SDK Components & Versions
| Component | Version |
|---|---|
| Linux Kernel | 4.19.73+ (2019 LTS) |
| U-Boot | 2019.01+ |
| Yocto Project | 2.6 (Thud) |
| Arm Toolchain (gcc) | 8.3-2019-03 hard-float |
| Qt | 5.11 |
| Wayland | 5.0 |
| GStreamer | 1.14.4 |
Component versions for M4/DSP builds
The toolchain for building M4/DSP firmware compatible with this version of Processor SDK Linux Automotive is automatically downloaded as part of Yocto recipes.
Supported Platforms
Supported Host Operating Systems
The following operating systems have been validated to work with our SDK. Note that only 64-bit host operating system is supported.
| Operating System | Version |
| Ubuntu | 18.04 (64-bit) |
Supported Platforms and EVMs
The following platforms and EVMs are supported with Processor SDK Linux Automotive.
| Platform | EVM | Silicon PG |
| DRA756 | Rev-H | PG 2.0 |
| DRA74x | Rev-H | PG 2.0 |
| DRA72x | Rev-C | PG 2.0 |
| DRA71x | Rev-A | PG 2.1 |
| DRA76x | Rev-B | PG 1.0 |
DRA71x and DRA76x are fully tested platforms. The other platforms go through a sanity test cycle to ensure that there are no regressions.
Defects and Known Issues
This section covers the open defects and known issues in this release. Defects correspond to bugs in SW. Major defects will be addressed either in subsequent LTS kernel release or through post-release updates.
Known issues are typically problems due to board limitations, invalid use cases, low probability/priority bugs, etc. No fixes are planned for known issues.
Limitations from last release
The following features are *not* present in this release as compared to the previous releases on K4.4:
- OpenCL, OpenCV
- FPDLink display
- FPDLink Capture
- Analog camera capture
- JAMR daughter card
Customers are expected to forward port these features from K4.4 to latest LTS version if needed. Please contact support if you have any questions on porting these patches.
Fixed in this release
| Key | Severity | Component | Summary |
| LCPD-13506 | S2-Major | Baseport | Updating boot0 partition through dfu causes timeouts in eMMC |
| LCPD-15479 | S2-Major | Audio & Display | DSS-WB Inconsistent behavior observed when converting to NM12 format |
| LCPD-16593 | S2-Major | Audio & Display | Errors observed for IOCTLs with DMABuf import/export capture operation |
| LCPD-16383 | S2-Major | Uboot | Uboot: Could not fatwrite to USB stick |
| LCPD-15547 | S2-Major | SATA | SATA read write tests failed |
| LCPD-15378 | S2-Major | Connectivity | SATA RX PHY config - update to match the DPLL output configuration |
| LCPD-15370 | S2-Major | Connectivity | Uboot SD card read write failed at size 8M and bigger |
| LCPD-15196 | S2-Major | Connectivity | u-boot configures VSDMMC rail for 3.0V instead of 3.3V |
| LCPD-14837 | S2-Major | Connectivity | U-boot: Increase allocated size for MLO.raw for DFU |
| LCPD-16096 | S2-Major | Audio & Display | Instability observed while trying to capture video with USB camera via Gstreamer |
| LCPD-14372 | S2-Major | Connectivity | Uboot mmc command shows "omap_hsmmc_send_cmd: timedout" error |
| LCPD-16007 | S2-Major | Connectivity | EVM USB device not detected by EVM host |
| LCPD-16181 | S2-Major | Connectivity | U-boot: DRA74: MMC3 does not have correct IODELAY values for DS, HS, SDR12, SDR25 |
| LCPD-15432 | S2-Major | Graphics | Wayland based demos hang if both HDMI and LCD are connected |
| LCPD-15384 | S2-Major | Graphics | Segmentation Fault and bad alloc errors observed when running GLMark2 |
| LCPD-14817 | S2-Major | Graphics | coredump in PVRSRVDestroyRecursiveMutex |
| LCPD-15386 | S2-Major | Graphics | Segmentation fault reported while running GC320 |
| LCPD-15260 | S2-Major | Multimedia | Video on display repeated when Fast Forward done with gst-play |
| LCPD-15259 | S2-Major | Multimedia | Gst-ducati fails to decode few interlaced streams |
| LCPD-15422 | S2-Major | Power & Thermal | cpuhotplug03 test failed |
| LCPD-15423 | S2-Major | Security | L3 Custom Error: MASTER MPU TARGET L4_PER1_P3 observed while running OPTEE tests |
| LCPD-16188 | S2-Major | System Integration | opencl/cv/mp/armnn, etc. dependencies broken for dra7xx-hs-evm |
| LCPD-15636 | S2-Major | System Integration | C++ compilation is not working |
| LCPD-15421 | S2-Major | System Integration | native compilation is not working |
| LCPD-15467 | S2-Major | System Test | MSI interrupt could not be enabled and no MSI interrupt entry in interrupt table |
| LCPD-15896 | S2-Major | Audio & Display | Suspend sometimes fails due to touch screen error (edt_ft5x06) |
| LCPD-14704 | S2-Major | Audio & Display | OMAPDRM: WARN seen after a suspend/resume cycle |
| LCPD-14703 | S2-Major | Audio & Display | VIP: Fix DT endpoint not bidirectional warning |
| LCPD-17083 | S2-Major | Audio & Display | DSS scaling sets error -ERANGE |
| LCPD-14553 | S2-Major | Baseport | dra72-evm: suspend triggers WARN from clockdomain |
| LCPD-15632 | S2-Major | Baseport | default console in uboot is set to ttyO2 instead of ttyO0 |
| LCPD-15459 | S2-Major | Baseport | rmmod/modprobe cycle fails for crypto modules |
| LCPD-12176 | S2-Major | Baseport | U-boot: Fix IOdelay error path issue |
| LCPD-15494 | S2-Major | Connectivity | dra7: pcie: PHY driver doesn't follow TRM power up sequence |
| LCPD-16618 | S2-Major | Connectivity | Uboot eMMC bus width is not 8-bit |
| LCPD-14824 | S2-Major | Graphics | Enabling PVR_DEBUG_MUTEXES option results in a compile error |
| LCPD-15373 | S2-Major | IPC | iommu/omap: include/linux/omap-iommu.h:30:10: error: 'ENOTSUP' undeclared |
| LCPD-14821 | S2-Major | IPC | net/rpmsg: rpmsg_sock_sendmsg() returning incorrect value on success |
Open Defects
| Key | Severity | Component | Summary |
| LCPD-15461 | S2-Major | Connectivity | pcie usb failed to enumerate sometimes on dra7xx |
| LCPD-16382 | S2-Major | Connectivity | pcie usb/sata read write tests failed |
| LCPD-17164 | S2-Major | Graphics | GLBenchmark is not able to run missing libgbm.so.2 error reported |
| LCPD-15918 | S2-Major | IPC | ti-ipc-rtos gets stuck in xdctools |
| LCPD-16556 | S2-Major | System Test | LMBENCH performance numbers lower than expected |
| LCPD-17342 | S2-Major | System Test | Dhrystone numbers look off in Performance Guide |
| LCPD-16642 | S2-Major | Audio & Display | omapdrm: in some cases, DPI output width does not need to be divisible by 8 |
| LCPD-15518 | S2-Major | Audio & Display | omapdrm: WB M2M: Headless mode is not working |
| LCPD-15540 | S2-Major | Connectivity | uvc-gadget results in segmentation fault |
| LCPD-17118 | S2-Major | Connectivity | Kernel MMC/SD user's guide incorrectly refers to OMAP-HSMMC |
| LCPD-16594 | S2-Major | Connectivity | Seeing kernel traces during pcie wifi tests |
| LCPD-15405 | S2-Major | Connectivity | DFU: could not update eMMC bootloaders when using dfu_alt_info_emmc set in uboot env |
| LCPD-15410 | S2-Major | Graphics | vdd_shv_power is ~200mw higher than on previous lts |
| LCPD-15794 | S3-Minor | Graphics | Allow non-root user access to graphics resources to enable graphics use case |
| LCPD-15400 | S2-Major | IPC | remoteproc/omap: System suspend fails for IPU1 domain without any remoteprocs loaded |
| LCPD-15402 | S2-Major | IPC | rpmsg-rpc: test application does not bail out gracefully upon error recovery |
Known Issues
| Key | Severity | Component | Summary | Impact | Workaround |
| PSDKLA-3398 | S2-Major | MMC/SD | Dra7xx-evm: Kernel stuck at omap_hsmmc 4809c000.mmc: card busy for almost 1 sec | "SD card is enumerated in ddr/high speed mode not UHS mode.Boot is delayed by almost 1sec" | Removing pull up resistor on MMC1 clock line reduces chances of hitting this issue. |
| PSDKLA-3383 | S2-Major | I2C | I2C3 support is not enabled in device tree file on dra71x-evm | ||
| LCPD-15635 | S2-Major | Connectivity | mmc hotplug causes one board reboot | ||
| LCPD-17373 | S2-Major | Power & Thermal | ARM Exception from PPA Signature Verification Call on HS Device | ||
| PSDKLA-5023 | S2-Major | Audio & Display | Late attach for DSP2 is not functional | "Observed only on some boards" | Remove timer13 from u-boot and dts file |
| PSDKLA-3382 | S2-Major | WLAN | BT Wilink support is not enabled in device tree file on dra71x-evm | ||
| PSDKLA-3855 | S2-Major | MMC/SD | DRA76x-EVM : SD card UHS modes are not supported on TI EVM due to regulator limitation | ||
| PSDKLA-1364 | S2-Major | ETH | DRA7xx(J6/J6Eco) : ethernet : reliability issues/link failure with gigabit mode of operation(on some boards) | "Observed only on specific boards" | Connect to 100 Mbps port |
| PSDKLA-3399 | S2-Major | MMC/SD | Stuck for 10-15 seconds on SD recovery | Userspace applications/console will be delayed by 10-15 sec as filesystem will not be mounted until the fs check is completed. | "Do not force power off/recycle the board. Use ""reboot"" command.or ""sync"" followed by ""halt""." |
| PSDKLA-3299 | S3-Minor | Audio & Display | DRA72x: FPDLink: Triple display usecase not functional | ||
| PSDKLA-3058 | S3-Minor | Audio & Display | Sluggish touch response with matrix-gui on Rev G DRA7xx EVM with LG display | ||
| PSDKLA-1387 | S3-Minor | ETH | DRA7xx : ethernet : 10Mbps mode does not work | "HW limitation on EVM" | None |
| LCPD-9402 | S2-Major | Audio & Display | DRA72x: HDMI display EDID read fails on Rev B EVM | When using Rev B EVM, EDID read will not work. This will result in the HDMI driver using the builtin modes in the kernel. HDMI will work at maximum of 1024x768 resolution. | Add the required HDMI modes into the kernel binary as per instructions in http://lxr.free-electrons.com/source/Documentation/EDID/ |
| LCPD-8000 | S2-Major | Audio & Display | VIP: RGB: RGB capture error due to wrong data path setting | ||
| LCPD-7374 | S2-Major | Connectivity | DRA7x: Transcend 16G UHS card enumerated as SDR104 but there are errors showing up | ||
| LCPD-9192 | S2-Major | Connectivity, Unknown | UART: DMA: data inconsistency observed with serial check utility on uart3 and glitches observed in BT playback | "One may hear glitches in Audio playback over Bluetooth." | None |
| LCPD-8352 | S2-Major | Graphics | weston: stress testing with 75 concurrent instances of simple-egl leads to unresponsive HMI due to running out of memory | oom-killer stops an application to free up memory. It could be either Wayland client or Weston itself. If Weston is killed, a board reboot would be required. | 1. Restart Wayland application. 2. Restart board if Weston is killed by oom-killer |
| LCPD-7255 | S2-Major | System Integration | Telnet login takes too long (~40 seconds) | "Booting with rootfs mounted over NFS might cause ~40 seconds delay on telnet login because DNS entries might not be properly populated. To work around this issue, enter appropriate DNS server IP in resolv.conf. For example: echo 'nameserver 192.0.2.2' > /etc/resolv.conf; " | |
| LCPD-7695 | S3-Minor | Audio & Display | DRA7xx: building Ov1603x as a module causes a green tint in captured image | "As this is only related to starting the capture within one second of insertine module. The impact is on the early video use cases." | The workround is to use the camera driver as builtin. Also, a delay of 1s can stop this issue from occuring |
| LCPD-9168 | S3-Minor | Audio & Display | Rotation using DSS/DRM TILER 2D not supported for NV12 and YUYV |
Installation and Usage
The Software Developer's Guide provides instructions on how to setup up your Linux development environment, install the SDK and start your development. It also includes User's Guides for various Example Applications.
Technical Support and Product Updates
Technical support is a broad term. Our desire is to provide a solid product, good documentation, and useful training that defines a clear path for developing a product based on the Linux/RTOS SDK. However, we know we'll never cover everything that can be done, and occasionally we even make mistakes <gasp>. So, when you can't seem to find what you need, there's a good place to search through previously answered questions and ask a new one - The E2E Support Forums. There is an active community of TIers and other customers like you already using a TI Processor, on these forums. You may find your question has already been answered with a quick Search of the Forums. If not, a quick post will likely provide you the answers you need.
We strongly recommend using the E2E for all queries.
There could be a few cases where your query has confidential information and cannot be posted publicly. In such cases, please contact your FAE or CPM.
Release Download
The latest release can be downloaded from this link
For earlier releases, go to Archives