|
|
#define | _SlFd_t Fd_t |
| |
| #define | sl_IfOpen spi_Open |
| | Opens an interface communication port to be used for communicating with a SimpleLink device. More...
|
| |
| #define | sl_IfClose spi_Close |
| | Closes an opened interface communication port. More...
|
| |
| #define | sl_IfRead spi_Read |
| | Attempts to read up to len bytes from an opened communication channel into a buffer starting at pBuff. More...
|
| |
| #define | sl_IfWrite spi_Write |
| | attempts to write up to len bytes to the SPI channel More...
|
| |
| #define | sl_IfRegIntHdlr(InterruptHdl, pValue) NwpRegisterInterruptHandler(InterruptHdl , pValue) |
| | register an interrupt handler routine for the host IRQ More...
|
| |
| #define | sl_IfMaskIntHdlr() NwpMaskInterrupt() |
| | Masks the Host IRQ. More...
|
| |
| #define | sl_IfUnMaskIntHdlr() NwpUnMaskInterrupt() |
| | Unmasks the Host IRQ. More...
|
| |
The SimpleLink device supports several standard communication protocol among SPI and
UART. CC32XX Host Driver implements SPI Communication Interface
- Note
- In CC32XX, SPI implementation uses DMA in order to increase the utilization of the communication channel. If user prefers to user UART, these interfaces need to be redefined
porting ACTION:
| #define sl_IfClose spi_Close |
Closes an opened interface communication port.
- Parameters
-
| fd | - file descriptor of opened communication channel |
- Returns
- upon successful completion, the function shall return 0. Otherwise, -1 shall be returned
- See Also
- sl_IfOpen , sl_IfRead , sl_IfWrite
- Note
- The prototype of the function is as follow: int xxx_IfClose(Fd_t Fd);
-
belongs to configuration_sec
- Warning
| #define sl_IfMaskIntHdlr |
( |
) | |
NwpMaskInterrupt() |
| #define sl_IfOpen spi_Open |
Opens an interface communication port to be used for communicating with a SimpleLink device.
Given an interface name and option flags, this function opens
the communication port and creates a file descriptor.
This file descriptor is used afterwards to read and write
data from and to this specific communication channel.
The speed, clock polarity, clock phase, chip select and all other
specific attributes of the channel are all should be set to hardcoded
in this function.
- Parameters
-
| ifName | - points to the interface name/path. The interface name is an optional attributes that the simple link driver receives on opening the driver (sl_Start). In systems that the spi channel is not implemented as part of the os device drivers, this parameter could be NULL. |
| flags | - optional flags parameters for future use |
- Returns
- upon successful completion, the function shall open the channel and return a non-negative integer representing the file descriptor. Otherwise, -1 shall be returned
- See Also
- sl_IfClose , sl_IfRead , sl_IfWrite
- Note
- The prototype of the function is as follow: Fd_t xxx_IfOpen(char* pIfName , unsigned long flags);
-
belongs to configuration_sec
- Warning
| #define sl_IfRead spi_Read |
Attempts to read up to len bytes from an opened communication channel into a buffer starting at pBuff.
- Parameters
-
| fd | - file descriptor of an opened communication channel |
| pBuff | - pointer to the first location of a buffer that contains enough space for all expected data |
| len | - number of bytes to read from the communication channel |
- Returns
- upon successful completion, the function shall return the number of read bytes. Otherwise, 0 shall be returned
- See Also
- sl_IfClose , sl_IfOpen , sl_IfWrite
- Note
- The prototype of the function is as follow: int xxx_IfRead(Fd_t Fd , char* pBuff , int Len);
-
belongs to configuration_sec
- Warning
| #define sl_IfRegIntHdlr |
( |
|
InterruptHdl, |
|
|
|
pValue |
|
) |
| NwpRegisterInterruptHandler(InterruptHdl , pValue) |
register an interrupt handler routine for the host IRQ
- Parameters
-
| InterruptHdl | - pointer to interrupt handler routine |
| pValue | - pointer to a memory structure that is passed to the interrupt handler. |
- Returns
- upon successful registration, the function shall return 0. Otherwise, -1 shall be returned
- See Also
- Note
- If there is already registered interrupt handler, the function should overwrite the old handler with the new one
-
If the handler is a null pointer, the function should un-register the interrupt handler, and the interrupts can be disabled.
-
belongs to configuration_sec
- Warning
| #define sl_IfUnMaskIntHdlr |
( |
) | |
NwpUnMaskInterrupt() |
Unmasks the Host IRQ.
- See Also
- sl_IfMaskIntHdlr
- Note
- belongs to configuration_sec
- Warning
| #define sl_IfWrite spi_Write |
attempts to write up to len bytes to the SPI channel
- Parameters
-
| fd | - file descriptor of an opened communication channel |
| pBuff | - pointer to the first location of a buffer that contains the data to send over the communication channel |
| len | - number of bytes to write to the communication channel |
- Returns
- upon successful completion, the function shall return the number of sent bytes. therwise, 0 shall be returned
- See Also
- sl_IfClose , sl_IfOpen , sl_IfRead
- Note
- This function could be implemented as zero copy and return only upon successful completion of writing the whole buffer, but in cases that memory allocation is not too tight, the function could copy the data to internal buffer, return back and complete the write in parallel to other activities as long as the other SPI activities would be blocked until the entire buffer write would be completed
The prototype of the function is as follow: int xxx_IfWrite(Fd_t Fd , char* pBuff , int Len);
- Note
- belongs to configuration_sec
- Warning