|
CC32XX SimpleLink Host Driver
1.0.0.10
|
Macros | |
| #define | SL_INC_ARG_CHECK |
| Defines whether the SimpleLink driver perform argument check or not. More... | |
| #define | SL_INC_STD_BSD_API_NAMING |
| Defines whether SimpleLink driver should expose standard BSD APIs or not. More... | |
| #define | SL_INC_EXT_API |
| Defines whether to include extended API in SimpleLink driver or not. More... | |
| #define | SL_INC_WLAN_PKG |
| Defines whether to include WLAN package in SimpleLink driver or not. More... | |
| #define | SL_INC_SOCKET_PKG |
| Defines whether to include SOCKET package in SimpleLink driver or not. More... | |
| #define | SL_INC_NET_APP_PKG |
| Defines whether to include NET_APP package in SimpleLink driver or not. More... | |
| #define | SL_INC_NET_CFG_PKG |
| Defines whether to include NET_CFG package in SimpleLink driver or not. More... | |
| #define | SL_INC_NVMEM_PKG |
| Defines whether to include NVMEM package in SimpleLink driver or not. More... | |
| #define | SL_INC_SOCK_SERVER_SIDE_API |
| Defines whether to include socket server side APIs in SimpleLink driver or not. More... | |
| #define | SL_INC_SOCK_CLIENT_SIDE_API |
| Defines whether to include socket client side APIs in SimpleLink driver or not. More... | |
| #define | SL_INC_SOCK_RECV_API |
| Defines whether to include socket receive APIs in SimpleLink driver or not. More... | |
| #define | SL_INC_SOCK_SEND_API |
| Defines whether to include socket send APIs in SimpleLink driver or not. More... | |
This section IS NOT REQUIRED in case one of the following pre defined capabilities set is in use:
PORTING ACTION:
| #define SL_INC_ARG_CHECK |
Defines whether the SimpleLink driver perform argument check or not.
When defined, the SimpleLink driver perform argument check on
function call. Removing this define could reduce some code
size and improve slightly the performances but may impact in
unpredictable behavior in case of invalid arguments
| #define SL_INC_EXT_API |
Defines whether to include extended API in SimpleLink driver or not.
When defined, the SimpleLink driver will include also all
exteded API of the included packages
| #define SL_INC_NET_APP_PKG |
Defines whether to include NET_APP package in SimpleLink driver or not.
When defined, the SimpleLink driver will include also the
NET_APP package
| #define SL_INC_NET_CFG_PKG |
Defines whether to include NET_CFG package in SimpleLink driver or not.
When defined, the SimpleLink driver will include also
the NET_CFG package
| #define SL_INC_NVMEM_PKG |
Defines whether to include NVMEM package in SimpleLink driver or not.
When defined, the SimpleLink driver will include also the
NVMEM package
| #define SL_INC_SOCK_CLIENT_SIDE_API |
Defines whether to include socket client side APIs in SimpleLink driver or not.
When defined, the SimpleLink driver will include also socket
client side APIs
| #define SL_INC_SOCK_RECV_API |
Defines whether to include socket receive APIs in SimpleLink driver or not.
When defined, the SimpleLink driver will include also socket
receive side APIs
| #define SL_INC_SOCK_SEND_API |
Defines whether to include socket send APIs in SimpleLink driver or not.
When defined, the SimpleLink driver will include also socket
send side APIs
| #define SL_INC_SOCK_SERVER_SIDE_API |
Defines whether to include socket server side APIs in SimpleLink driver or not.
When defined, the SimpleLink driver will include also socket
server side APIs
| #define SL_INC_SOCKET_PKG |
Defines whether to include SOCKET package in SimpleLink driver or not.
When defined, the SimpleLink driver will include also
the SOCKET package
| #define SL_INC_STD_BSD_API_NAMING |
Defines whether SimpleLink driver should expose standard BSD APIs or not.
When defined, the SimpleLink driver in addtion to its alternative
BSD APIs expose also standard BSD APIs.
Stadrad BSD API includs the following functions:
socket , close , accept , bind , listen , connect , select ,
setsockopt , getsockopt , recv , recvfrom , write , send , sendto ,
gethostbyname
| #define SL_INC_WLAN_PKG |
Defines whether to include WLAN package in SimpleLink driver or not.
When defined, the SimpleLink driver will include also
the WLAN package