![]() |
CC3200 Peripheral Driver Library User's Guide
1.2.0
|
Functions | |
| void | PRCMMCUReset (tBoolean bIncludeSubsystem) |
| unsigned long | PRCMSysResetCauseGet () |
| void | PRCMPeripheralClkEnable (unsigned long ulPeripheral, unsigned long ulClkFlags) |
| void | PRCMPeripheralClkDisable (unsigned long ulPeripheral, unsigned long ulClkFlags) |
| unsigned long | PRCMPeripheralClockGet (unsigned long ulPeripheral) |
| void | PRCMPeripheralReset (unsigned long ulPeripheral) |
| tBoolean | PRCMPeripheralStatusGet (unsigned long ulPeripheral) |
| void | PRCMI2SClockFreqSet (unsigned long ulI2CClkFreq) |
| void | PRCMLPDSRestoreInfoSet (unsigned long ulStackPtr, unsigned long ulProgCntr) |
| void | PRCMLPDSEnter () |
| void | PRCMLPDSEnterKeepDebugIf () |
| void | PRCMLPDSWakeupSourceEnable (unsigned long ulLpdsWakeupSrc) |
| void | PRCMLPDSWakeupSourceDisable (unsigned long ulLpdsWakeupSrc) |
| unsigned long | PRCMLPDSWakeupCauseGet () |
| void | PRCMLPDSIntervalSet (unsigned long ulTicks) |
| void | PRCMLPDSWakeUpGPIOSelect (unsigned long ulGPIOPin, unsigned long ulType) |
| void | PRCMSleepEnter () |
| void | PRCMSRAMRetentionEnable (unsigned long ulSramColSel, unsigned long ulModeFlags) |
| void | PRCMSRAMRetentionDisable (unsigned long ulSramColSel, unsigned long ulFlags) |
| void | PRCMHibernateWakeupSourceEnable (unsigned long ulHIBWakupSrc) |
| void | PRCMHibernateWakeupSourceDisable (unsigned long ulHIBWakupSrc) |
| unsigned long | PRCMHibernateWakeupCauseGet () |
| void | PRCMHibernateIntervalSet (unsigned long long ullTicks) |
| void | PRCMHibernateWakeUpGPIOSelect (unsigned long ulGPIOBitMap, unsigned long ulType) |
| void | PRCMHibernateEnter () |
| unsigned long long | PRCMSlowClkCtrGet () |
| unsigned long long | PRCMSlowClkCtrFastGet (void) |
| void | PRCMSlowClkCtrMatchSet (unsigned long long ullValue) |
| unsigned long long | PRCMSlowClkCtrMatchGet () |
| void | PRCMOCRRegisterWrite (unsigned char ucIndex, unsigned long ulRegValue) |
| unsigned long | PRCMOCRRegisterRead (unsigned char ucIndex) |
| void | PRCMIntRegister (void(*pfnHandler)(void)) |
| void | PRCMIntUnregister () |
| void | PRCMIntEnable (unsigned long ulIntFlags) |
| void | PRCMIntDisable (unsigned long ulIntFlags) |
| unsigned long | PRCMIntStatus () |
| void | PRCMRTCInUseSet () |
| tBoolean | PRCMRTCInUseGet () |
| void | PRCMRTCSet (unsigned long ulSecs, unsigned short usMsec) |
| void | PRCMRTCGet (unsigned long *ulSecs, unsigned short *usMsec) |
| void | PRCMRTCMatchSet (unsigned long ulSecs, unsigned short usMsec) |
| void | PRCMRTCMatchGet (unsigned long *ulSecs, unsigned short *usMsec) |
| void | PRCMCC3200MCUInit () |
| unsigned long | PRCMHIBRegRead (unsigned long ulRegAddr) |
| void | PRCMHIBRegWrite (unsigned long ulRegAddr, unsigned long ulValue) |
| unsigned long | PRCMCameraFreqSet (unsigned char ulDivider, unsigned char ulWidth) |
| unsigned long PRCMCameraFreqSet | ( | unsigned char | ulDivider, |
| unsigned char | ulWidth | ||
| ) |
| ulDivider | is clock frequency divider value |
| ulWidth | is the width of the high pulse |
This function sets the input frequency for camera module.
The frequency is calculated as follows:
f_out = 240MHz/ulDivider;
The parameter ulWidth sets the width of the high pulse.
For e.g.:
ulDivider = 4; ulWidth = 2; f_out = 30 MHz and 50% duty cycle
And,
ulDivider = 4; ulWidth = 1; f_out = 30 MHz and 25% duty cycle
| void PRCMCC3200MCUInit | ( | void | ) |
MCU Initialization Routine
This function sets mandatory configurations for the MCU
| void PRCMHibernateEnter | ( | void | ) |
Puts the system into Hibernate
This function puts the system into Hibernate. The device enters HIB immediately and on exit from HIB device core starts its execution from reset thus the function never returns.
| void PRCMHibernateIntervalSet | ( | unsigned long long | ullTicks | ) |
Sets Hibernate wakeup Timer
| ullTicks | is number of 32.768 KHz clocks |
This function sets internal hibernate wakeup timer running at 32.768 KHz.
| unsigned long PRCMHibernateWakeupCauseGet | ( | void | ) |
Get hibernate wakeup cause
This function gets the hibernate wakeup cause.
| void PRCMHibernateWakeUpGPIOSelect | ( | unsigned long | ulGPIOBitMap, |
| unsigned long | ulType | ||
| ) |
Selects the GPIO(s) for hibernate wakeup
| ulGPIOBitMap | is the bit-map of valid hibernate wakeup GPIO. |
| ulType | is the wakeup trigger type. |
This function setects the wakeup GPIO for hibernate and can be used to select any combination of 7 pre-defined GPIO(s).
This function enables individual HIB wakeup source(s). The paramter ulGPIOBitMap should be one of the follwoing :- -PRCM_HIB_GPIO2 -PRCM_HIB_GPIO4 -PRCM_HIB_GPIO13 -PRCM_HIB_GPIO17 -PRCM_HIB_GPIO11 -PRCM_HIB_GPIO24 -PRCM_HIB_GPIO26
The parameter ulType sets the trigger type and can be one of the following:
| void PRCMHibernateWakeupSourceDisable | ( | unsigned long | ulHIBWakupSrc | ) |
Disable individual HIB wakeup source(s).
| ulHIBWakupSrc | is logical OR of valid HIB wakeup sources. |
This function disable individual HIB wakeup source(s). The paramter ulHIBWakupSrc is same as bit fileds defined in PRCMEnableHibernateWakeupSource()
| void PRCMHibernateWakeupSourceEnable | ( | unsigned long | ulHIBWakupSrc | ) |
Enables individual HIB wakeup source(s).
| ulHIBWakupSrc | is logical OR of valid HIB wakeup sources. |
This function enables individual HIB wakeup source(s). The paramter ulHIBWakupSrc is the bit mask of HIB wakeup sources and should be logical OR of one or more of the follwoing :- -PRCM_HIB_SLOW_CLK_CTR -PRCM_HIB_GPIO2 -PRCM_HIB_GPIO4 -PRCM_HIB_GPIO13 -PRCM_HIB_GPIO17 -PRCM_HIB_GPIO11 -PRCM_HIB_GPIO24 -PRCM_HIB_GPIO26
| unsigned long PRCMHIBRegRead | ( | unsigned long | ulRegAddr | ) |
Reads 32-bit value from register at specified address
| ulRegAddr | is the address of register to be read. |
This function reads 32-bit value from the register as specified by ulRegAddr.
| void PRCMHIBRegWrite | ( | unsigned long | ulRegAddr, |
| unsigned long | ulValue | ||
| ) |
Writes 32-bit value to register at specified address
| ulRegAddr | is the address of register to be read. |
| ulValue | is the 32-bit value to be written. |
This function writes 32-bit value passed as ulValue to the register as specified by ulRegAddr
| void PRCMI2SClockFreqSet | ( | unsigned long | ulI2CClkFreq | ) |
Configure I2S fracactional divider
| ulI2CClkFreq | is the required input clock for McAPS module |
This function configures I2S fractional divider. By default this divider is set to output 24 Mhz clock to I2S module.
The minimum frequency that can be obtained by configuring this divider is
(240000KHz/1023.99) = 234.377 KHz
| void PRCMIntDisable | ( | unsigned long | ulIntFlags | ) |
Disables individual PRCM interrupt sources.
| ulIntFlags | is the bit mask of the interrupt sources to be disabled. |
This function disables the indicated ARCM interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The ulIntFlags parameter has the same definition as the ulIntFlags parameter to PRCMEnableInterrupt().
| void PRCMIntEnable | ( | unsigned long | ulIntFlags | ) |
Enables individual PRCM interrupt sources.
| ulIntFlags | is the bit mask of the interrupt sources to be enabled. |
This function enables the indicated ARCM interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The ulIntFlags parameter is the logical OR of any of the following: -PRCM_INT_SLOW_CLK_CTR
| void PRCMIntRegister | ( | void(*)(void) | pfnHandler | ) |
Registers an interrupt handler for the PRCM.
| pfnHandler | is a pointer to the function to be called when the interrupt is activated. |
This function does the actual registering of the interrupt handler. This function enables the global interrupt in the interrupt controller;
| unsigned long PRCMIntStatus | ( | void | ) |
Gets the current interrupt status.
This function returns the PRCM interrupt status of interrupts that are allowed to reflect to the processor. The interrupts are cleared on read.
| void PRCMIntUnregister | ( | void | ) |
Unregisters an interrupt handler for the PRCM.
This function does the actual unregistering of the interrupt handler. It clears the handler to be called when a PRCM interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
| void PRCMLPDSEnter | ( | void | ) |
Puts the system into Low Power Deel Sleep (LPDS) power mode.
This function puts the system into Low Power Deel Sleep (LPDS) power mode. A call to this function never returns and the execution starts from Reset.
| void PRCMLPDSEnterKeepDebugIf | ( | void | ) |
Puts the system into Low Power Deel Sleep (LPDS) power mode keeping debug interface alive.
This function puts the system into Low Power Deel Sleep (LPDS) power mode keeping debug interface alive. A call to this function never returns and the execution starts from Reset
| void PRCMLPDSIntervalSet | ( | unsigned long | ulTicks | ) |
Sets LPDS wakeup Timer
| ulTicks | is number of 32.768 KHz clocks |
This function sets internal LPDS wakeup timer running at 32.768 KHz. The timer is only configured if the parameter ulTicks is in valid range i.e. from 21 to 2^32.
| void PRCMLPDSRestoreInfoSet | ( | unsigned long | ulStackPtr, |
| unsigned long | ulProgCntr | ||
| ) |
Sets the LPDS exit PC and SP restore vlaues.
| ulStackPtr | is the SP restore value. |
| ulProgCntr | is the PC restore value |
This function sets the LPDS exit PC and SP restore vlaues. Setting ulProgCntr to a non-zero value, forces bootloader to jump to that address with Stack Pointer initialized to ulStackPtr on LPDS exit, otherwise the application's vector table entries are used.
| unsigned long PRCMLPDSWakeupCauseGet | ( | void | ) |
Get LPDS wakeup cause
This function gets LPDS wakeup caouse
| void PRCMLPDSWakeUpGPIOSelect | ( | unsigned long | ulGPIOPin, |
| unsigned long | ulType | ||
| ) |
Selects the GPIO for LPDS wakeup
| ulGPIOPin | is one of the valid GPIO fro LPDS wakeup. |
| ulType | is the wakeup trigger type. |
This function setects the wakeup GPIO for LPDS wakeup and can be used to select one out of 7 pre-defined GPIO(s).
The parameter ulLpdsGPIOSel should be one of the following:- -PRCM_LPDS_GPIO2 -PRCM_LPDS_GPIO4 -PRCM_LPDS_GPIO13 -PRCM_LPDS_GPIO17 -PRCM_LPDS_GPIO11 -PRCM_LPDS_GPIO24 -PRCM_LPDS_GPIO26
The parameter ulType sets the trigger type and can be one of the following:
| void PRCMLPDSWakeupSourceDisable | ( | unsigned long | ulLpdsWakeupSrc | ) |
Disable the individual LPDS wakeup source(s).
| ulLpdsWakeupSrc | is logical OR of wakeup sources. |
This function enable the individual LPDS wakeup source(s) and following three wake up sources (ulLpdsWakeupSrc ) are supported by the device. -PRCM_LPDS_HOST_IRQ -PRCM_LPDS_GPIO -PRCM_LPDS_TIMER
| void PRCMLPDSWakeupSourceEnable | ( | unsigned long | ulLpdsWakeupSrc | ) |
Enable the individual LPDS wakeup source(s).
| ulLpdsWakeupSrc | is logical OR of wakeup sources. |
This function enable the individual LPDS wakeup source(s) and following three wakeup sources (ulLpdsWakeupSrc ) are supported by the device. -PRCM_LPDS_HOST_IRQ -PRCM_LPDS_GPIO -PRCM_LPDS_TIMER
| void PRCMMCUReset | ( | tBoolean | bIncludeSubsystem | ) |
Performs a software reset of a MCU and associated peripherals
| bIncludeSubsystem | is true to reset associated peripherals. |
This function performs a software reset of a MCU and associated peripherals. To reset the associated peripheral, the parameter bIncludeSubsystem should be set to true.
| unsigned long PRCMOCRRegisterRead | ( | unsigned char | ucIndex | ) |
Read from On-Chip Retention (OCR) register.
This function reads from On-Chip retention register. The device supports two 4-byte OCR register which are retained across all power mode.
The parameter ucIndex is an index of the OCR and can be 0 or 1.
| void PRCMOCRRegisterWrite | ( | unsigned char | ucIndex, |
| unsigned long | ulRegValue | ||
| ) |
Write to On-Chip Retention (OCR) register.
This function writes to On-Chip retention register. The device supports two 4-byte OCR register which are retained across all power mode.
The parameter ucIndex is an index of the OCR and can be 0 or 1.
| void PRCMPeripheralClkDisable | ( | unsigned long | ulPeripheral, |
| unsigned long | ulClkFlags | ||
| ) |
Disables clock(s) to peripheral.
| ulPeripheral | is one of the valid peripherals |
| ulClkFlags | are bitmask of clock(s) to be enabled. |
This function disable the clock for the specified peripheral. Peripherals are by default clock gated (disabled) and generated a bus fault if accessed.
The parameter ulClkFlags can be logical OR bit fields as defined in PRCMEnablePeripheral().
| void PRCMPeripheralClkEnable | ( | unsigned long | ulPeripheral, |
| unsigned long | ulClkFlags | ||
| ) |
Enable clock(s) to peripheral.
| ulPeripheral | is one of the valid peripherals |
| ulClkFlags | are bitmask of clock(s) to be enabled. |
This function enables the clock for the specified peripheral. Peripherals are by default clock gated (disabled) and generates a bus fault if accessed.
The parameter ulClkFlags can be logical OR of the following: -PRCM_RUN_MODE_CLK - Ungates clock to the peripheral -PRCM_SLP_MODE_CLK - Keeps the clocks ungated in sleep.
| unsigned long PRCMPeripheralClockGet | ( | unsigned long | ulPeripheral | ) |
Gets the input clock for the specified peripheral.
| ulPeripheral | is one of the valid peripherals. |
This function gets the input clock for the specified peripheral.
The parameter ulPeripheral has the same definition as that in PRCMPeripheralClkEnable();
| void PRCMPeripheralReset | ( | unsigned long | ulPeripheral | ) |
Performs a software reset of a peripheral.
| ulPeripheral | is one of the valid peripheral. |
This assert or deassert reset to the specified peripheral based of the bAssert parameter.
| tBoolean PRCMPeripheralStatusGet | ( | unsigned long | ulPeripheral | ) |
Determines if a peripheral is ready.
| ulPeripheral | is one of the valid modules |
This function determines if a particular peripheral is ready to be accessed. The peripheral may be in a non-ready state if it is not enabled, is being held in reset, or is in the process of becoming ready after being enabled or taken out of reset.
| void PRCMRTCGet | ( | unsigned long * | ulSecs, |
| unsigned short * | usMsec | ||
| ) |
Get the instantaneous calendar time from the device.
| ulSecs | refers to the seconds part of the calendar time |
| usMsec | refers to the fractional (ms) part of the second |
This function fetches the instantaneous value of the ticking calendar time from the device. The calendar time is outlined in terms of seconds and milliseconds.
The device provides the calendar value that has been maintained across active and low power states.
The function PRCMRTCSet() must have been invoked once to set a reference.
| tBoolean PRCMRTCInUseGet | ( | void | ) |
Ascertain whether function of RTC is being used
This function indicates whether function of RTC is being used on the device or not.
This routine should be utilized by the application software, when returning from low-power, to confirm that RTC has been put to use and may not need to set the value of the RTC.
The RTC feature, if set or marked, can be only reset either through reboot or power cycle.
| void PRCMRTCInUseSet | ( | void | ) |
Mark the function of RTC as being used
This function marks in HW that feature to maintain calendar time in device is being used.
Specifically, this feature reserves user's HIB Register-1 accessed through PRCMOCRRegisterWrite(1) for internal work / purpose, therefore, the stated register is not available to user. Also, users must not excercise the Slow Clock Counter API(s), if RTC has been set for use.
The RTC feature, if set or marked, can be only reset either through reboot or power cycle.
| void PRCMRTCMatchGet | ( | unsigned long * | ulSecs, |
| unsigned short * | usMsec | ||
| ) |
Get a previously set calendar time alarm.
| ulSecs | refers to the seconds part of the calendar time |
| usMsec | refers to the fractional (ms) part of the second |
This function fetches from the device a wall-clock alarm that would have been previously set in the device. The calendar time is outlined in terms of seconds and milliseconds.
If no alarm was set in the past, then this function would fetch a random information.
The function PRCMRTCMatchSet() must have been invoked once to set an alarm.
| void PRCMRTCMatchSet | ( | unsigned long | ulSecs, |
| unsigned short | usMsec | ||
| ) |
Set a calendar time alarm.
| ulSecs | refers to the seconds part of the calendar time |
| usMsec | refers to the fractional (ms) part of the second |
This function sets an wall-clock alarm in the device to be reported for a futuristic calendar time. The calendar time is outlined in terms of seconds and milliseconds.
The device provides uses the calendar value that has been maintained across active and low power states to report attainment of alarm time.
The function PRCMRTCSet() must have been invoked once to set a reference.
| void PRCMRTCSet | ( | unsigned long | ulSecs, |
| unsigned short | usMsec | ||
| ) |
Set the calendar time in the device.
| ulSecs | refers to the seconds part of the calendar time |
| usMsec | refers to the fractional (ms) part of the second |
This function sets the specified calendar time in the device. The calendar time is outlined in terms of seconds and milliseconds. However, the device makes no assumption about the origin or reference of the calendar time.
The device uses the indicated calendar value to update and maintain the wall-clock time across active and low power states.
The function PRCMRTCInUseSet() must be invoked prior to use of this feature.
| void PRCMSleepEnter | ( | void | ) |
Puts the system into Sleep.
This function puts the system into sleep power mode. System exits the power state on any one of the available interrupt. On exit from sleep mode the function returns to the calling function with all the processor core registers retained.
| unsigned long long PRCMSlowClkCtrFastGet | ( | void | ) |
Gets the current value of the internal slow clock counter
This function is similar to
| unsigned long long PRCMSlowClkCtrGet | ( | void | ) |
Gets the current value of the internal slow clock counter
This function latches and reads the internal RTC running at 32.768 Khz
| unsigned long long PRCMSlowClkCtrMatchGet | ( | void | ) |
Gets slow clock counter match value.
This function gets the match value for slow clock counter. This is use to interrupt the processor when RTC counts to the specified value.
| void PRCMSlowClkCtrMatchSet | ( | unsigned long long | ullValue | ) |
Sets slow clock counter match value to interrupt the processor.
| ullValue | is the match value. |
This function sets the match value for slow clock counter. This is use to interrupt the processor when RTC counts to the specified value.
| void PRCMSRAMRetentionDisable | ( | unsigned long | ulSramColSel, |
| unsigned long | ulFlags | ||
| ) |
Disable SRAM column retention during LPDS Power mode(s).
| ulSramColSel | is bit mask of valid SRAM columns. |
| ulFlags | is the bit mask of power modes. |
This functions disable the SRAM retention. The device supports configurable SRAM column retention in Low Power Deep Sleep (LPDS). Each column is of 64 KB size.
The parameter ulSramColSel should be logical OR of the following:- -PRCM_SRAM_COL_1 -PRCM_SRAM_COL_2 -PRCM_SRAM_COL_3 -PRCM_SRAM_COL_4
The parameter ulFlags selects the power modes and sholud be logical OR of one or more of the following -PRCM_SRAM_LPDS_RET
| void PRCMSRAMRetentionEnable | ( | unsigned long | ulSramColSel, |
| unsigned long | ulModeFlags | ||
| ) |
Enable SRAM column retention during LPDS Power mode(s)
| ulSramColSel | is bit mask of valid SRAM columns. |
| ulModeFlags | is the bit mask of power modes. |
This functions enables the SRAM retention. The device supports configurable SRAM column retention in Low Power Deep Sleep (LPDS). Each column is of 64 KB size.
The parameter ulSramColSel should be logical OR of the following:- -PRCM_SRAM_COL_1 -PRCM_SRAM_COL_2 -PRCM_SRAM_COL_3 -PRCM_SRAM_COL_4
The parameter ulModeFlags selects the power modes and sholud be logical OR of one or more of the following -PRCM_SRAM_LPDS_RET
| unsigned long PRCMSysResetCauseGet | ( | void | ) |
Gets the reason for a reset.
This function returns the reason(s) for a reset. The reset reason are:- -PRCM_POWER_ON - Device is powering up. -PRCM_LPDS_EXIT - Device is exiting from LPDS. -PRCM_CORE_RESET - Device is exiting soft core only reset -PRCM_MCU_RESET - Device is exiting soft subsystem reset. -PRCM_WDT_RESET - Device was reset by watchdog. -PRCM_SOC_RESET - Device is exting SOC reset. -PRCM_HIB_EXIT - Device is exiting hibernate.