![]() |
CC3200 Peripheral Driver Library User's Guide
1.2.0
|
Functions | |
void | ADCEnable (unsigned long ulBase) |
void | ADCDisable (unsigned long ulBase) |
void | ADCChannelEnable (unsigned long ulBase, unsigned long ulChannel) |
void | ADCChannelDisable (unsigned long ulBase, unsigned long ulChannel) |
void | ADCIntRegister (unsigned long ulBase, unsigned long ulChannel, void(*pfnHandler)(void)) |
void | ADCIntUnregister (unsigned long ulBase, unsigned long ulChannel) |
void | ADCIntEnable (unsigned long ulBase, unsigned long ulChannel, unsigned long ulIntFlags) |
void | ADCIntDisable (unsigned long ulBase, unsigned long ulChannel, unsigned long ulIntFlags) |
unsigned long | ADCIntStatus (unsigned long ulBase, unsigned long ulChannel) |
void | ADCIntClear (unsigned long ulBase, unsigned long ulChannel, unsigned long ulIntFlags) |
void | ADCDMAEnable (unsigned long ulBase, unsigned long ulChannel) |
void | ADCDMADisable (unsigned long ulBase, unsigned long ulChannel) |
void | ADCTimerConfig (unsigned long ulBase, unsigned long ulValue) |
void | ADCTimerReset (unsigned long ulBase) |
void | ADCTimerEnable (unsigned long ulBase) |
void | ADCTimerDisable (unsigned long ulBase) |
unsigned long | ADCTimerValueGet (unsigned long ulBase) |
unsigned char | ADCFIFOLvlGet (unsigned long ulBase, unsigned long ulChannel) |
unsigned long | ADCFIFORead (unsigned long ulBase, unsigned long ulChannel) |
void ADCChannelDisable | ( | unsigned long | ulBase, |
unsigned long | ulChannel | ||
) |
Disables specified ADC channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channelsber |
This function disables specified ADC channel.
void ADCChannelEnable | ( | unsigned long | ulBase, |
unsigned long | ulChannel | ||
) |
Enables specified ADC channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels |
This function enables specified ADC channel and configures the pin as analog pin.
void ADCDisable | ( | unsigned long | ulBase | ) |
Disable the ADC
ulBase | is the base address of the ADC |
This function clears the ADC global enable
void ADCDMADisable | ( | unsigned long | ulBase, |
unsigned long | ulChannel | ||
) |
Disables the ADC DMA operation for specified channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels |
This function disables the DMA operation for specified ADC channel
The parameter ulChannel should be one of the following
void ADCDMAEnable | ( | unsigned long | ulBase, |
unsigned long | ulChannel | ||
) |
Enables the ADC DMA operation for specified channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels |
This function enables the DMA operation for specified ADC channel
The parameter ulChannel should be one of the following
void ADCEnable | ( | unsigned long | ulBase | ) |
Enables the ADC
ulBase | is the base address of the ADC |
This function sets the ADC global enable
unsigned char ADCFIFOLvlGet | ( | unsigned long | ulBase, |
unsigned long | ulChannel | ||
) |
Gets the current FIFO level for specified ADC channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels. |
This function returns the current FIFO level for specified ADC channel.
The parameter ulChannel should be one of the following
unsigned long ADCFIFORead | ( | unsigned long | ulBase, |
unsigned long | ulChannel | ||
) |
Reads FIFO for specified ADC channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels. |
This function returns one data sample from the channel fifo as specified by ulChannel parameter.
The parameter ulChannel should be one of the following
void ADCIntClear | ( | unsigned long | ulBase, |
unsigned long | ulChannel, | ||
unsigned long | ulIntFlags | ||
) |
Clears the current channel interrupt sources
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels |
ulIntFlags | is the bit mask of the interrupt sources to be cleared. |
This function clears individual interrupt source for the specified ADC channel.
The parameter ulChannel should be as explained in
void ADCIntDisable | ( | unsigned long | ulBase, |
unsigned long | ulChannel, | ||
unsigned long | ulIntFlags | ||
) |
Disables individual interrupt sources for specified channel
ulBase | is the base address of the ADC. |
ulChannel | is one of the valid ADC channels |
ulIntFlags | is the bit mask of the interrupt sources to be enabled. |
This function disables the indicated ADC interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The parametersulIntFlags and ulChannel should be as explained in ADCIntEnable().
void ADCIntEnable | ( | unsigned long | ulBase, |
unsigned long | ulChannel, | ||
unsigned long | ulIntFlags | ||
) |
Enables individual interrupt sources for specified channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels |
ulIntFlags | is the bit mask of the interrupt sources to be enabled. |
This function enables the indicated ADC interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The parameter ulChannel should be one of the following
The ulIntFlags parameter is the logical OR of any of the following:
void ADCIntRegister | ( | unsigned long | ulBase, |
unsigned long | ulChannel, | ||
void(*)(void) | pfnHandler | ||
) |
Enables and registers ADC interrupt handler for specified channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels |
pfnHandler | is a pointer to the function to be called when the ADC channel interrupt occurs. |
This function enables and registers ADC interrupt handler for specified channel. Individual interrupt for each channel should be enabled using
The parameter ulChannel should be one of the following
unsigned long ADCIntStatus | ( | unsigned long | ulBase, |
unsigned long | ulChannel | ||
) |
Gets the current channel interrupt status
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels |
This function returns the interrupt status of the specified ADC channel.
The parameter ulChannel should be as explained in
void ADCIntUnregister | ( | unsigned long | ulBase, |
unsigned long | ulChannel | ||
) |
Disables and unregisters ADC interrupt handler for specified channel
ulBase | is the base address of the ADC |
ulChannel | is one of the valid ADC channels |
This function disables and unregisters ADC interrupt handler for specified channel. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
The parameter ulChannel should be one of the following
void ADCTimerConfig | ( | unsigned long | ulBase, |
unsigned long | ulValue | ||
) |
Configures the ADC internal timer
ulBase | is the base address of the ADC |
ulValue | is wrap arround value of the timer |
This function Configures the ADC internal timer. The ADC timer is a 17 bit used to timestamp the ADC data samples internally. User can read the timestamp along with the sample from the FIFO register(s). Each sample in the FIFO contains 14 bit actual data and 18 bit timestamp
The parameter ulValue can take any value between 0 - 2^17
void ADCTimerDisable | ( | unsigned long | ulBase | ) |
Disables ADC internal timer
ulBase | is the base address of the ADC |
This function disables 17-bit ADC internal timer
void ADCTimerEnable | ( | unsigned long | ulBase | ) |
Enables ADC internal timer
ulBase | is the base address of the ADC |
This function enables 17-bit ADC internal timer
void ADCTimerReset | ( | unsigned long | ulBase | ) |
Resets ADC internal timer
ulBase | is the base address of the ADC |
This function resets 17-bit ADC internal timer
unsigned long ADCTimerValueGet | ( | unsigned long | ulBase | ) |
Gets the current value of ADC internal timer
ulBase | is the base address of the ADC |
This function the current value of 17-bit ADC internal timer