SYS/BIOS
7.00
|
CC26xx Boot Support.
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
Go to the source code of this file.
Functions | |
void | Boot_trimDevice (void) |
Trim device flag; determines if SetupTrimDevice() is called at boot, default is true. More... | |
uint32_t | Boot_getBootReason (void) |
Gets the reason for the most recent boot of the CPU. More... | |
void Boot_trimDevice | ( | void | ) |
Trim device flag; determines if SetupTrimDevice() is called at boot, default is true.
Set to false to disable the Boot module from trimming the device. The device must be trimmed for proper operation. If the Boot module doesn't do this, the application must explicitly call SetupTrimDevice().
uint32_t Boot_getBootReason | ( | void | ) |
Gets the reason for the most recent boot of the CPU.
SysCtrlResetSourceGet() DriverLib API.
The | reset reason, as reported by the |