#include </home/developer/.conan/data/tirtos/7.03.00.10/library-sb/ga/build/5ab84d6acfe1f23c4fae0ab88f26e3a396351ac9/kernel/tirtos7/packages/ti/sysbios/heaps/HeapMultiBuf.h>
§ iheap
IHeap_Object HeapMultiBuf_Struct::iheap |
§ objElem
§ blockBorrow
bool HeapMultiBuf_Struct::blockBorrow |
Turn block borrowing on (true) or off (false)
With block borrowing on, if there are no blocks available of the requested size, then alloc will look for a larger block to return. Calls to alloc which borrow blocks will be slower, and will cause internal fragmentation of the heap (until the block is freed), so it is ideal to configure a HeapMultiBuf such that block borrowing is not needed.
§ numHeapBufs
int HeapMultiBuf_Struct::numHeapBufs |
§ numBufs
int HeapMultiBuf_Struct::numBufs |
Number of memory buffers.
The number of different fixed size memory buffers that are managed by the heap instance. The bufParams array has length numBufs.
The default number of buffers is 0.
§ bufsBySize
§ bufsByAddr
HeapMultiBuf_AddrPair* HeapMultiBuf_Struct::bufsByAddr |
The documentation for this struct was generated from the following file:
- /home/developer/.conan/data/tirtos/7.03.00.10/library-sb/ga/build/5ab84d6acfe1f23c4fae0ab88f26e3a396351ac9/kernel/tirtos7/packages/ti/sysbios/heaps/HeapMultiBuf.h