![]() |
![]() |
SYS/BIOS
7.00
|
Data Fields | |
char * | buf |
Buffer that will be managed by the heap instance. More... | |
size_t | size |
Size (in MADUs) of the heap. More... | |
char* HeapMin_Params::buf |
Buffer that will be managed by the heap instance.
When creating a heap at runtime, the user must supply the memory that the heap will manage. It is up to the caller to align the buffer as needed.
This parameter is ignored when creating heaps during configuration.
size_t HeapMin_Params::size |
Size (in MADUs) of the heap.
This parameter specifies the size of the heap managed by a HeapMin
instance. In the static case, a buffer of length size
will be created. In the dynamic case, size
specifies the size of the buffer (i.e. parameter buf
) that the caller provides.
This is a required parameter. It must be set by the caller. Failure to do so will result in an Assert (if BIOS.assertsEnabled config parameter is true).