355 #define do_hwi_undef_short_names 356 #define do_hwi_short_to_long_name_conversion 357 #include "Hwi_defs.h" 360 #ifndef ti_sysbios_family_arm_v6m_Hwi__include 361 #define ti_sysbios_family_arm_v6m_Hwi__include 377 #define Hwi_E_badIntNum "intnum: %d is out of range" 382 #define Hwi_E_alreadyDefined "Hwi already defined: intr# %d" 388 #define Hwi_E_hwiLimitExceeded "Too many interrupts defined" 393 #define Hwi_E_exception "hardware exception id = %d, pc = 0x%08x" 398 #define Hwi_E_noIsr "no ISR, id = %d, pc = 0x%08x" 403 #define Hwi_E_NMI "NMI: %s" 408 #define Hwi_E_hardFault "Hard-fault: %s" 413 #define Hwi_E_memFault "Mem-fault: %s, addresss: 0x%08x" 418 #define Hwi_E_busFault "Bus-fault: %s, address: 0x%08x" 423 #define Hwi_E_usageFault "Usage-fault: %s" 428 #define Hwi_E_svCall "SvCall: svNum = %d" 433 #define Hwi_E_debugMon "Debug-monitor: %s" 438 #define Hwi_E_reserved "reserved %s %d" 443 #define Hwi_E_stackOverflow "ISR stack overflow" 453 typedef struct Hwi_Struct2__ Hwi_Struct2__;
570 uint8_t USERSETMPEND;
571 uint8_t NONEBASETHRDENA;
586 uint32_t RES_20 [56];
588 uint32_t RES_120 [24];
590 uint32_t RES_1A0 [24];
592 uint32_t RES_220 [24];
594 uint32_t RES_2A0 [24];
596 uint32_t RES_320 [56];
598 uint32_t RES_4F0 [516];
630 uint32_t RES_D8C[93];
632 uint32_t RES_F04[12];
638 uint32_t RES_F48[34];
757 extern const bool Hwi_dispatcherAutoNestingSupport;
774 extern const bool Hwi_dispatcherSwiSupport;
791 extern const bool Hwi_dispatcherTaskSupport;
806 extern const bool Hwi_dispatcherIrpTrackingSupport;
981 extern const uint32_t Hwi_ccr;
1135 extern void Hwi_init(
void);
1141 extern void Hwi_Instance_finalize(
Hwi_Object *obj,
int ec);
1289 extern bool Hwi_getCoreStackInfo(
Hwi_StackInfo *stkInfo,
bool computeStackDepth,
unsigned int coreId);
1298 extern void Hwi_startup(
void);
1304 extern void Hwi_switchFromBootStack(
void);
1312 extern void Hwi_post(
unsigned int intNum);
1322 extern char *Hwi_getTaskSP(
void);
1451 extern void Hwi_plug(
unsigned int intNum,
void *fxn);
1476 extern void Hwi_setPriority(
unsigned int intNum,
unsigned int priority);
1496 extern Hwi_Handle Hwi_construct2(Hwi_Struct2 *hwi,
int intNum,
Hwi_FuncPtr hwiFxn,
const Hwi_Params *prms);
1497 extern void Hwi_initNVIC(
void);
1498 extern void Hwi_initStacks(
void * hwiStack);
1500 extern void Hwi_excHandlerAsm(
void);
1501 extern void Hwi_excHandler(
unsigned int *excStack,
unsigned int lr);
1502 extern void Hwi_excHandlerMin(
unsigned int *excStack,
unsigned int lr);
1503 extern void Hwi_excHandlerMax(
unsigned int *excStack,
unsigned int lr);
1504 extern void Hwi_excFillContext(
unsigned int *excStack);
1505 extern void Hwi_excNmi(
unsigned int *excStack);
1506 extern void Hwi_excHardFault(
unsigned int *excStack);
1507 extern void Hwi_excMemFault(
unsigned int *excStack);
1508 extern void Hwi_excBusFault(
unsigned int *excStack);
1509 extern void Hwi_excUsageFault(
unsigned int *excStack);
1510 extern void Hwi_excSvCall(
unsigned int *excStack);
1511 extern void Hwi_excDebugMon(
unsigned int *excStack);
1512 extern void Hwi_excReserved(
unsigned int *excStack,
unsigned int excNum);
1513 extern void Hwi_excNoIsr(
unsigned int *excStack,
unsigned int excNum);
1514 extern void Hwi_excDumpRegs(
unsigned int lr);
1515 extern void Hwi_pendSV(
void);
1516 extern void Hwi_setStackLimit(
void * stackBase);
1517 extern unsigned int Hwi_swiDisableNull(
void);
1518 extern void Hwi_swiRestoreNull(
unsigned int key);
1519 extern void Hwi_dispatch(
void);
1520 extern unsigned int Hwi_dispatchC(uintptr_t irp, uint32_t dummy1, uint32_t dummy2,
Hwi_Object *hwi);
1521 extern void Hwi_doSwiRestore(
unsigned int tskKey);
1522 extern void Hwi_doTaskRestore(
unsigned int tskKey);
1523 extern unsigned int Hwi_swiDisable();
1524 extern void Hwi_swiRestore(
unsigned int key);
1525 extern void Hwi_swiRestoreHwi(
unsigned int key);
1526 extern unsigned int Hwi_taskDisable();
1527 extern void Hwi_taskRestoreHwi(
unsigned int key);
1535 extern void Hwi_switchFromBootStack(
void);
1538 extern void Hwi_checkStack(
void);
1541 extern void Hwi_initStack(
void);
1544 extern void Hwi_initStackMin(
void);
1575 #define Hwi_module ((Hwi_Module_State *) &(Hwi_Module_state)) 1577 #define Hwi_Object_heap() NULL 1579 static inline Hwi_Handle Hwi_handle(
Hwi_Struct *str)
1581 return ((Hwi_Handle)str);
1584 static inline Hwi_Struct * Hwi_struct(Hwi_Handle h)
1597 #if defined(ti_sysbios_family_arm_v6m_Hwi__nolocalnames) 1598 #define do_hwi_undef_short_names 1599 #include "Hwi_defs.h" void * r0
Definition: Hwi.h:667
void * hwiStackBase
Definition: Hwi.h:549
void Hwi_destruct(Hwi_Struct *obj)
uint32_t PID0
Definition: Hwi.h:643
const int Hwi_NUM_INTERRUPTS
The Cortex M0 NVIC supports up to 256 interrupts/exceptions.
bool enableInt
Enable this interrupt when object is created? Default is true.
Definition: Hwi.h:997
void * BFAR
Definition: Hwi.h:691
uint32_t PID2
Definition: Hwi.h:645
uint8_t * intAffinity
Definition: Hwi.h:708
void Hwi_setFunc(Hwi_Handle hwi, Hwi_FuncPtr fxn, uintptr_t arg)
Overwrite Hwi function and arg.
void(* deleteFxn)(Hwi_Handle arg1)
Definition: Hwi.h:514
uint8_t MMFSR
Definition: Hwi.h:607
uint32_t ISAR1
Definition: Hwi.h:624
int priority
Interrupt priority.
Definition: Hwi.h:1014
Hwi_Handle Hwi_getHandle(unsigned int intNum)
Returns Hwi_handle associated with intNum.
void(* Hwi_ExcHandlerFuncPtr)(unsigned int *arg1, unsigned int arg2)
Hwi exception handler function type definition.
Definition: Hwi.h:739
BIOS_ThreadType
Current thread type definitions.
Definition: BIOS.h:189
const unsigned int Hwi_numSparseInterrupts
If Hwi.dispatchTableSize is initialized by the user then Hwi.numSparseInterrupts is set to the value ...
uint32_t AIRCR
Definition: Hwi.h:602
size_t hwiStackPeak
Definition: Hwi.h:547
uint32_t CID1
Definition: Hwi.h:648
uint32_t BFAR
Definition: Hwi.h:613
uint16_t UFSR
Definition: Hwi.h:609
uint32_t SHCSR
Definition: Hwi.h:606
uint32_t CPACR
Definition: Hwi.h:629
const unsigned int Hwi_priGroup
The PRIGROUP setting. Default is 0.
void * excStack
Definition: Hwi.h:700
void * r9
Definition: Hwi.h:676
void * MMFSR
Definition: Hwi.h:685
void * dispatchTable
Definition: Hwi.h:706
void ** hookEnv
Definition: Hwi.h:733
char * taskSP
Definition: Hwi.h:697
uint32_t SCR
Definition: Hwi.h:603
void * UFSR
Definition: Hwi.h:687
void * r7
Definition: Hwi.h:674
void * r5
Definition: Hwi.h:672
uint32_t STRVR
Definition: Hwi.h:583
volatile Hwi_NVIC Hwi_nvic
Physical Nested Vectored Interrupt Controller Device. short name is "Hwi_nvic" long name is "ti_sysbi...
uint32_t VTOR
Definition: Hwi.h:601
void Hwi_setHookContext(Hwi_Handle hwi, int id, void *hookContext)
Set hook instance's context for a Hwi.
unsigned int Hwi_Disable()
Globally disable interrupts.
uint8_t priority
Interrupt priority.
Definition: Hwi.h:731
void Hwi_excSetBuffers(void *excContextBuffer, void *excStackBuffer)
Set the exception context and stack buffer pointers.
uint32_t FPCCR
Definition: Hwi.h:633
uint32_t PID6
Definition: Hwi.h:641
uint32_t PFR0
Definition: Hwi.h:615
uint32_t MVFR0
Definition: Hwi.h:636
uint32_t MMFR0
Definition: Hwi.h:619
Only this interrupt is disabled (not support on cortexM devices)
Definition: Hwi.h:529
Hwi_Struct * Hwi_Instance
Definition: Hwi.h:448
void * vectorTableBase
Definition: Hwi.h:705
unsigned int Hwi_Enable()
Globally enable interrupts.
void * ICSR
Definition: Hwi.h:684
All interrupts are disabled (not support on cortexM devices)
Definition: Hwi.h:527
bool Hwi_getStackInfo(Hwi_StackInfo *stkInfo, bool computeStackDepth)
Get Hwi stack usage Info.
uint32_t STCSR
Definition: Hwi.h:582
void * r3
Definition: Hwi.h:670
void * r1
Definition: Hwi.h:668
uint32_t ISAR2
Definition: Hwi.h:625
size_t hwiStackSize
Definition: Hwi.h:548
bool useDispatcher
Use the interrupt dispatcher with this interrupt. Default is true.
Definition: Hwi.h:1034
bool initDone
Definition: Hwi.h:711
All current and lower priority interrupts are disabled. (default for all cortexM devices) ...
Definition: Hwi.h:533
void Hwi_Restore(uint32_t key)
restore global interrupts to the state they were in prior Hwi_disable().
void Hwi_switchAndRunFunc(void(*func)(void))
uint32_t FPCAR
Definition: Hwi.h:634
void * r6
Definition: Hwi.h:673
unsigned int Hwi_enableInterrupt(unsigned int intNum)
Enable a specific interrupt.
void * BFSR
Definition: Hwi.h:686
Hwi_Handle Hwi_create(int intNum, Hwi_FuncPtr hwiFxn, const Hwi_Params *prms, Error_Block *eb)
uint32_t PID7
Definition: Hwi.h:642
uint32_t DFR0
Definition: Hwi.h:617
void(* Hwi_FuncPtr)(uintptr_t)
Hwi create function type definition.
Definition: Hwi.h:486
const unsigned int Hwi_disablePriority
The priority that BASEPRI is set to by Hwi_disable().
uint32_t RES_08
Definition: Hwi.h:580
User supplies interrupt enable masks (not support on cortexM devices)
Definition: Hwi.h:531
void * HFSR
Definition: Hwi.h:688
uint32_t CID3
Definition: Hwi.h:650
void * r2
Definition: Hwi.h:669
uint32_t PID4
Definition: Hwi.h:639
Hwi_MaskingOption
Interrupt masking options.
Definition: Hwi.h:523
void * excContext
Definition: Hwi.h:699
const int Hwi_NUM_PRIORITIES
The Cortex M0 NVIC supports up to 256 interrupt priorities.
void Hwi_delete(Hwi_Handle *handle)
void Hwi_post(unsigned int intNum)
Generate an interrupt for test purposes.
Hwi_Handle Hwi_Object_next(Hwi_Object *obj)
Hwi_Handle Hwi_construct(Hwi_Struct *obj, int intNum, Hwi_FuncPtr hwiFxn, const Hwi_Params *prms, Error_Block *eb)
uint32_t ISAR4
Definition: Hwi.h:627
No interrupts are disabled (not support on cortexM devices)
Definition: Hwi.h:525
void * r10
Definition: Hwi.h:677
uint32_t MMFR3
Definition: Hwi.h:622
unsigned int Hwi_disableInterrupt(unsigned int intNum)
Disable a specific interrupt.
uint32_t ICTR
Definition: Hwi.h:579
uint32_t CCR
Definition: Hwi.h:604
SYS/BIOS Top-Level Manager.
void * pc
Definition: Hwi.h:682
Error block.
Definition: Error.h:152
void Hwi_Params_init(Hwi_Params *prms)
void * sp
Definition: Hwi.h:680
void(* Hwi_VectorFuncPtr)(void)
Hwi vector function type definition.
Definition: Hwi.h:491
uint32_t ISAR0
Definition: Hwi.h:623
void * r12
Definition: Hwi.h:679
void * MMAR
Definition: Hwi.h:690
void * AFSR
Definition: Hwi.h:692
void * DFSR
Definition: Hwi.h:689
uint8_t BFSR
Definition: Hwi.h:608
Nested Vectored Interrupt Controller.
Definition: Hwi.h:577
uint32_t CPUIDBR
Definition: Hwi.h:599
void(* beginFxn)(Hwi_Handle arg1)
Definition: Hwi.h:512
Hwi_FuncPtr fxn
Definition: Hwi.h:720
void(* endFxn)(Hwi_Handle arg1)
Definition: Hwi.h:513
uint32_t ICSR
Definition: Hwi.h:600
void Hwi_reconfig(Hwi_Handle hwi, Hwi_FuncPtr fxn, const Hwi_Params *params)
Reconfigure a dispatched interrupt.
Hwi_FuncPtr Hwi_getFunc(Hwi_Handle hwi, uintptr_t *arg)
Get Hwi function and arg.
uint32_t FPDSCR
Definition: Hwi.h:635
uintptr_t irp
Definition: Hwi.h:721
uintptr_t arg
ISR function argument. Default is 0.
Definition: Hwi.h:719
int length
Definition: Hwi.h:517
uint32_t AFR0
Definition: Hwi.h:618
uint32_t PID3
Definition: Hwi.h:646
int eventId
Interrupt event ID (Interrupt Selection Number)
Definition: Hwi.h:1004
void * psr
Definition: Hwi.h:683
uint32_t AFSR
Definition: Hwi.h:614
BIOS_ThreadType threadType
Definition: Hwi.h:663
void Hwi_plug(unsigned int intNum, void *fxn)
Plug a non dispatched interrupt vector with an ISR address.
volatile bool vnvicFlushRequired
Definition: Hwi.h:707
void Hwi_restoreInterrupt(unsigned int intNum, unsigned int key)
Restore a specific interrupt's enabled/disabled state.
uint32_t DFSR
Definition: Hwi.h:611
void * isrStackSize
Definition: Hwi.h:704
Exception Context - Register contents at the time of an exception.
Definition: Hwi.h:662
void * isrStackBase
Definition: Hwi.h:702
void Hwi_setPriority(unsigned int intNum, unsigned int priority)
Set an interrupt's relative priority.
uint32_t PID5
Definition: Hwi.h:640
Hwi_VectorFuncPtr * vectorTable
Definition: Hwi.h:710
Hwi_Struct * Hwi_Handle
Definition: Hwi.h:447
uint32_t MMFR1
Definition: Hwi.h:620
uint32_t STCVR
Definition: Hwi.h:584
uint32_t MMAR
Definition: Hwi.h:612
unsigned int swiTaskKeys
Definition: Hwi.h:703
const Hwi_ExcHookFunc Hwi_excHookFunc
User Exception hook function.
Hwi_MaskingOption maskSetting
maskSetting. Default is Hwi_MaskingOption "Hwi_MaskingOption_SELF"
Definition: Hwi.h:989
uint32_t MVFR1
Definition: Hwi.h:637
void(* registerFxn)(int arg1)
Definition: Hwi.h:510
uint32_t RES_0C
Definition: Hwi.h:581
void * threadHandle
Definition: Hwi.h:664
uintptr_t arg
ISR function argument. Default is 0.
Definition: Hwi.h:993
Hwi_Handle Hwi_Object_first(void)
uint32_t STI
Definition: Hwi.h:631
uint32_t CID2
Definition: Hwi.h:649
uint32_t CID0
Definition: Hwi.h:647
void * Hwi_getHookContext(Hwi_Handle hwi, int id)
Get hook instance's context for a Hwi.
Hwi header file for the HAL.
size_t threadStackSize
Definition: Hwi.h:666
uintptr_t Hwi_getIrp(Hwi_Handle hwi)
Get address of interrupted instruction.
void * lr
Definition: Hwi.h:681
Structure contains Hwi stack usage info.
Definition: Hwi.h:546
int16_t intNum
Definition: Hwi.h:732
uint32_t ISAR3
Definition: Hwi.h:626
void * r8
Definition: Hwi.h:675
uint32_t RES_00
Definition: Hwi.h:578
void * r11
Definition: Hwi.h:678
uint32_t STCALIB
Definition: Hwi.h:585
void * r4
Definition: Hwi.h:671
void(* createFxn)(Hwi_Handle arg1, Error_Block *arg2)
Definition: Hwi.h:511
uint32_t MMFR2
Definition: Hwi.h:621
void(* Hwi_ExceptionHookFuncPtr)(Hwi_ExcContext *arg1)
Exception hook function type definition.
Definition: Hwi.h:496
bool excActive
Definition: Hwi.h:698
void * threadStack
Definition: Hwi.h:665
Hwi hook set type definition.
Definition: Hwi.h:509
uint32_t PFR1
Definition: Hwi.h:616
void Hwi_clearInterrupt(unsigned int intNum)
Clear a specific interrupt.
void * isrStack
Definition: Hwi.h:701
uint32_t HFSR
Definition: Hwi.h:610
uint32_t * intAffinityMasks
Definition: Hwi.h:709
uint32_t PID1
Definition: Hwi.h:644
Hwi_ExceptionHookFuncPtr Hwi_ExcHookFunc
Definition: Hwi.h:499