![]() |
![]() |
SYS/BIOS
7.00
|
A heap that calls user supplied callback functions.
The HeapCallback module enables users to provide a custom heap implementation by providing callback functions that will be invoked by HeapCallback for the various heap management functions.
The user-supplied HeapCallback.initInstFxn is called during boot time to initialize any HeapCallback objects that were created in the .cfg file. The user-supplied HeapCallback.createInstFxn is called during runtime for any calls to HeapCallback_create(). Both of these functions return a context value (typically a pointer to an object managed by the user-supplied heap code). This context value is passed to subsequent user allocInstFxn, freeInstFxn, etc. functions.
HeapCallback_alloc(), HeapCallback_free() and HeapCallback_getStats() call the user-supplied allocInstFxn, freeInstFxn and getStatsInstFxn functions with the context value returned by initInstFxn or createInstFxn.
HeapCallback_delete() calls the user-supplied instDeleteFxn with the context returned by the createInstFxn.
Configuration example: The following XDC configuration statements creates a HeapCallback instance and plugs in the user defined functions.
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/runtime/Error.h>
#include <ti/sysbios/runtime/IHeap.h>
#include <ti/sysbios/runtime/Memory.h>
Go to the source code of this file.
Data Structures | |
struct | HeapCallback_Params |
struct | HeapCallback_Struct |
Macros | |
#define | ti_sysbios_heaps_HeapCallback_Handle_upCast(handle) ((IHeap_Handle)(handle)) |
cast handle to an IHeap_Handle for use by Memory_alloc, etc. More... | |
Typedefs | |
typedef void *(* | HeapCallback_AllocInstFxn) (uintptr_t context, size_t size, size_t align) |
Instance alloc callback function signature. More... | |
typedef uintptr_t(* | HeapCallback_CreateInstFxn) (uintptr_t arg) |
Instance create callback function signature. More... | |
typedef void(* | HeapCallback_DeleteInstFxn) (uintptr_t context) |
Instance delete callback function signature. More... | |
typedef void(* | HeapCallback_FreeInstFxn) (uintptr_t context, void *addr, size_t size) |
Instance free callback function signature. More... | |
typedef void(* | HeapCallback_GetStatsInstFxn) (uintptr_t context, Memory_Stats *stats) |
Instance getStats callback function signature. More... | |
typedef bool(* | HeapCallback_IsBlockingInstFxn) (uintptr_t context) |
Instance isblocking callback function signature. More... | |
typedef struct HeapCallback_Struct * | HeapCallback_Handle |
typedef HeapCallback_Struct | HeapCallback_Object |
#define ti_sysbios_heaps_HeapCallback_Handle_upCast | ( | handle | ) | ((IHeap_Handle)(handle)) |
cast handle to an IHeap_Handle for use by Memory_alloc, etc.
handle | heap handle |
IHeap_Handle |
typedef void*(* HeapCallback_AllocInstFxn) (uintptr_t context, size_t size, size_t align) |
Instance alloc callback function signature.
This function takes the context return from createInstFxn(), the size to be allocated and the align value. The return value from this function is a pointer to the allocated memory block.
typedef uintptr_t(* HeapCallback_CreateInstFxn) (uintptr_t arg) |
Instance create callback function signature.
The 'arg' is passed as an argument to this function. The return value from this function (context) will be passed as an argument to the other instance functions.
typedef void(* HeapCallback_DeleteInstFxn) (uintptr_t context) |
Instance delete callback function signature.
The context returned from createInstFxn() is passed as an argument to this function.
typedef void(* HeapCallback_FreeInstFxn) (uintptr_t context, void *addr, size_t size) |
Instance free callback function signature.
This function takes the context returned by createInstFxn() and a pointer to the buffer to be freed and the size to be freed.
typedef void(* HeapCallback_GetStatsInstFxn) (uintptr_t context, Memory_Stats *stats) |
Instance getStats callback function signature.
This function takes the context returned by createInstFxn() and a pointer to a memory stats object.
typedef bool(* HeapCallback_IsBlockingInstFxn) (uintptr_t context) |
Instance isblocking callback function signature.
The context return from createInstFxn() is passed as an argument to this function. The return value is 'true' or 'false'.
typedef struct HeapCallback_Struct * HeapCallback_Handle |
void* HeapCallback_alloc | ( | HeapCallback_Handle | handle, |
size_t | size, | ||
size_t | align, | ||
Error_Block * | eb | ||
) |
Allocate a block of memory from the heap.
void HeapCallback_free | ( | HeapCallback_Handle | handle, |
void * | buf, | ||
size_t | size | ||
) |
Free a block of memory back to the heap.
bool HeapCallback_isBlocking | ( | HeapCallback_Handle | handle | ) |
Can this heap block the caller.
HeapCallback
returns true
if the configured callback heap can block. HeapCallback
returns false
if the configured callback heap cannot block.
handle | heap handle |
always | returns false |
void HeapCallback_getStats | ( | HeapCallback_Handle | handle, |
Memory_Stats * | stats | ||
) |
get memory stats for a HeapCallback object
handle | heap handle |
stats | pointer to a Memory_Stats object |
HeapCallback_Handle HeapCallback_create | ( | const HeapCallback_Params * | params, |
Error_Block * | eb | ||
) |
Create a HeapCallback
heap.
params | optional parameters |
eb | error block |
HeapMin | handle (NULL on failure) |
HeapCallback_Handle HeapCallback_construct | ( | HeapCallback_Struct * | obj, |
const HeapCallback_Params * | params | ||
) |
Construct a HeapCallback
heap.
HeapCallback_construct is equivalent to HeapCallback_create except that the HeapCallback_Struct is pre-allocated.
obj | pointer to a HeapCallback object |
params | optional parameters |
HeapCallback | handle (NULL on failure) |
void HeapCallback_delete | ( | HeapCallback_Handle * | handle | ) |
Delete a HeapCallback
heap.
Note that HeapCallback_delete takes a pointer to a HeapCallback_Handle which enables HeapCallback_delete to set the HeapCallback handle to NULL.
handle | pointer to a HeapCallback handle |
void HeapCallback_destruct | ( | HeapCallback_Struct * | obj | ) |
Destruct a HeapCallback
heap.
obj | pointer to a HeapCallback objects |
void HeapCallback_Params_init | ( | HeapCallback_Params * | prms | ) |
Initialize the HeapCallback_Params structure with default values.
HeapCallback_Params_init initializes the HeapCallback_Params structure with default values. HeapCallback_Params_init should always be called before setting individual parameter fields. This allows new fields to be added in the future with compatible defaults – existing source code does not need to change when new fields are added.
prms | pointer to uninitialized params structure |
HeapCallback_Handle HeapCallback_Object_first | ( | void | ) |
return handle of the first HeapCallback on HeapCallback list
Return the handle of the first HeapCallback on the create/construct list. NULL if no HeapCallbacks have been created or constructed.
HeapCallback | handle |
HeapCallback_Handle HeapCallback_Object_next | ( | HeapCallback_Handle | heap | ) |
return handle of the next HeapCallback on HeapCallback list
Return the handle of the next HeapCallback on the create/construct list. NULL if no more HeapCallbacks are on the list.
heap | HeapCallback handle |
HeapCallback | handle |
|
inlinestatic |
|
inlinestatic |