SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
OtaArchive_BundleFileInfo_t Struct Reference

Data Fields

uint8_t FileNameBuf [MAX_FILE_NAME_SIZE]
 
uint8_t CertificateFileNameBuf [MAX_FILE_NAME_SIZE]
 
uint8_t SignatureBuf [MAX_SIGNATURE_SIZE]
 
uint32_t SignatureLen
 
uint8_t Sha256Digest [MAX_SHA256_DIGEST_SIZE]
 
uint16_t Sha256DigestLen
 
uint32_t Secured
 
uint32_t Bundle
 
uint8_t SavedInFS
 

Detailed Description

Definition at line 85 of file OtaArchive.h.

Field Documentation

§ Bundle

uint32_t Bundle

Definition at line 94 of file OtaArchive.h.

§ CertificateFileNameBuf

uint8_t CertificateFileNameBuf[MAX_FILE_NAME_SIZE]

Definition at line 88 of file OtaArchive.h.

§ FileNameBuf

uint8_t FileNameBuf[MAX_FILE_NAME_SIZE]

Definition at line 87 of file OtaArchive.h.

§ SavedInFS

uint8_t SavedInFS

Definition at line 95 of file OtaArchive.h.

§ Secured

uint32_t Secured

Definition at line 93 of file OtaArchive.h.

§ Sha256Digest

uint8_t Sha256Digest[MAX_SHA256_DIGEST_SIZE]

Definition at line 91 of file OtaArchive.h.

§ Sha256DigestLen

uint16_t Sha256DigestLen

Definition at line 92 of file OtaArchive.h.

§ SignatureBuf

uint8_t SignatureBuf[MAX_SIGNATURE_SIZE]

Definition at line 89 of file OtaArchive.h.

§ SignatureLen

uint32_t SignatureLen

Definition at line 90 of file OtaArchive.h.


The documentation for this struct was generated from the following file: