Data Fields
UDMACC32XX_Config Struct Reference

UDMACC32XX Global configuration. More...

#include <UDMACC32XX.h>

Data Fields

void * object
 
void const * hwAttrs
 

Detailed Description

UDMACC32XX Global configuration.

The UDMACC32XX_Config structure contains pointers used by the UDMACC32XX driver.

This structure needs to be defined before calling UDMACC32XX_init() and it must not be changed thereafter.

Field Documentation

§ object

void* UDMACC32XX_Config::object

Pointer to UDMACC32XX object

§ hwAttrs

void const* UDMACC32XX_Config::hwAttrs

Pointer to hardware attributes


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale