Data Fields
SDHostCC32XX_Object Struct Reference

SDHostCC32XX Object. More...

#include <SDHostCC32XX.h>

Collaboration diagram for SDHostCC32XX_Object:
Collaboration graph
[legend]

Data Fields

volatile uint32_t rca
 
volatile uint32_t sectorCount
 
volatile uint32_t * buffer
 
SemaphoreP_Handle cmdSem
 
HwiP_Handle hwiHandle
 
UDMACC32XX_Handle dmaHandle
 
unsigned int powerMgrId
 
Power_NotifyObj postNotify
 
PowerCC32XX_ParkState prevParkCLK
 
uint16_t clkPin
 
volatile int_fast8_t stat
 
bool isOpen
 
bool ping
 
bool dmaPosted
 
SD_CardType cardType
 

Detailed Description

SDHostCC32XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ rca

volatile uint32_t SDHostCC32XX_Object::rca

§ sectorCount

volatile uint32_t SDHostCC32XX_Object::sectorCount

§ buffer

volatile uint32_t* SDHostCC32XX_Object::buffer

§ cmdSem

SemaphoreP_Handle SDHostCC32XX_Object::cmdSem

§ hwiHandle

HwiP_Handle SDHostCC32XX_Object::hwiHandle

§ dmaHandle

UDMACC32XX_Handle SDHostCC32XX_Object::dmaHandle

§ powerMgrId

unsigned int SDHostCC32XX_Object::powerMgrId

§ postNotify

Power_NotifyObj SDHostCC32XX_Object::postNotify

§ prevParkCLK

PowerCC32XX_ParkState SDHostCC32XX_Object::prevParkCLK

§ clkPin

uint16_t SDHostCC32XX_Object::clkPin

§ stat

volatile int_fast8_t SDHostCC32XX_Object::stat

§ isOpen

bool SDHostCC32XX_Object::isOpen

§ ping

bool SDHostCC32XX_Object::ping

§ dmaPosted

bool SDHostCC32XX_Object::dmaPosted

§ cardType

SD_CardType SDHostCC32XX_Object::cardType

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale