Data Fields
SDHostCC32XX_HWAttrsV1 Struct Reference

#include <SDHostCC32XX.h>

Data Fields

uint_fast32_t clkRate
 
int_fast32_t intPriority
 
uint_fast32_t baseAddr
 
unsigned long rxChIdx
 
unsigned long txChIdx
 
uint32_t dataPin
 
uint32_t cmdPin
 
uint32_t clkPin
 

Field Documentation

§ clkRate

uint_fast32_t SDHostCC32XX_HWAttrsV1::clkRate

SD interface clock rate

§ intPriority

int_fast32_t SDHostCC32XX_HWAttrsV1::intPriority

Internal SDHost ISR command/transfer priorty

§ baseAddr

uint_fast32_t SDHostCC32XX_HWAttrsV1::baseAddr

SDHost Peripheral base address

§ rxChIdx

unsigned long SDHostCC32XX_HWAttrsV1::rxChIdx

uDMA controlTable receive channel index

§ txChIdx

unsigned long SDHostCC32XX_HWAttrsV1::txChIdx

uDMA controlTable transmit channel index

§ dataPin

uint32_t SDHostCC32XX_HWAttrsV1::dataPin

SD Host Data pin

§ cmdPin

uint32_t SDHostCC32XX_HWAttrsV1::cmdPin

SD Host CMD pin

§ clkPin

uint32_t SDHostCC32XX_HWAttrsV1::clkPin

SD Host CLK pin


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale