Data Fields
I2CCC32XX_Object Struct Reference

I2CCC32XX Object. More...

#include <I2CCC32XX.h>

Collaboration diagram for I2CCC32XX_Object:
Collaboration graph
[legend]

Data Fields

I2C_BASE_OBJECT uint16_t burstCount
 
bool burstStarted
 
I2C_BitRate bitRate
 
Power_NotifyObj notifyObj
 

Detailed Description

I2CCC32XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ burstCount

I2C_BASE_OBJECT uint16_t I2CCC32XX_Object::burstCount

§ burstStarted

bool I2CCC32XX_Object::burstStarted

§ bitRate

I2C_BitRate I2CCC32XX_Object::bitRate

§ notifyObj

Power_NotifyObj I2CCC32XX_Object::notifyObj

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale