Data Fields
CaptureCC32XX_Object Struct Reference

CaptureCC32XX_Object. More...

#include <CaptureCC32XX.h>

Collaboration diagram for CaptureCC32XX_Object:
Collaboration graph
[legend]

Data Fields

HwiP_Handle hwiHandle
 
Power_NotifyObj notifyObj
 
Capture_CallBackFxn callBack
 
Capture_PeriodUnits periodUnits
 
uint32_t mode
 
uint32_t timer
 
uint32_t previousCount
 
bool isRunning
 

Detailed Description

CaptureCC32XX_Object.

The application must not access any member variables of this structure!

Field Documentation

§ hwiHandle

HwiP_Handle CaptureCC32XX_Object::hwiHandle

§ notifyObj

Power_NotifyObj CaptureCC32XX_Object::notifyObj

§ callBack

Capture_CallBackFxn CaptureCC32XX_Object::callBack

§ periodUnits

Capture_PeriodUnits CaptureCC32XX_Object::periodUnits

§ mode

uint32_t CaptureCC32XX_Object::mode

§ timer

uint32_t CaptureCC32XX_Object::timer

§ previousCount

uint32_t CaptureCC32XX_Object::previousCount

§ isRunning

bool CaptureCC32XX_Object::isRunning

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale