Data Structures | Macros | Typedefs | Variables
CameraCC32XXDMA.h File Reference

Detailed Description

Camera driver implementation for a CC32XX Camera controller.

============================================================================

The Camera header file should be included in an application as follows:

#include <ti/drivers/Camera/CameraCC32XXDMA.h>

Refer to Camera.h for a complete description of APIs & example of use.


#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/Camera.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
Include dependency graph for CameraCC32XXDMA.h:

Go to the source code of this file.

Data Structures

struct  CameraCC32XXDMA_HWAttrs
 CameraCC32XXDMA Hardware attributes. More...
 
struct  CameraCC32XXDMA_Object
 CameraCC32XXDMA Object. More...
 

Macros

#define CameraCC32XXDMA_DMA_TRANSFER_SIZE   64
 

Typedefs

typedef struct CameraCC32XXDMA_ObjectCameraCC32XXDMA_Handle
 

Variables

const Camera_FxnTable CameraCC32XXDMA_fxnTable
 

Macro Definition Documentation

§ CameraCC32XXDMA_DMA_TRANSFER_SIZE

#define CameraCC32XXDMA_DMA_TRANSFER_SIZE   64

Typedef Documentation

§ CameraCC32XXDMA_Handle

Variable Documentation

§ CameraCC32XXDMA_fxnTable

const Camera_FxnTable CameraCC32XXDMA_fxnTable
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale