![]() |
SimpleLink CC32xx ATCommands Library
Simplifies the implementation of Internet connectivity
|
Controls MQTT Client programming options and capabilities. More...
Functions | |
int32_t | ATCmdMqtt_createCallback (void *arg) |
Mqtt Client Create callback. More... | |
int32_t | ATCmdMqtt_deleteCallback (void *arg) |
Mqtt Client delete callback. More... | |
int32_t | ATCmdMqtt_connectCallback (void *arg) |
Mqtt Client Connect callback. More... | |
int32_t | ATCmdMqtt_disconnectCallback (void *arg) |
Mqtt Client Disconnect callback. More... | |
int32_t | ATCmdMqtt_publishCallback (void *arg) |
Mqtt Client Publish callback. More... | |
int32_t | ATCmdMqtt_subscribeCallback (void *arg) |
Mqtt Client Subscribe callback. More... | |
int32_t | ATCmdMqtt_unsubscribeCallback (void *arg) |
Mqtt Client Unsubscribe callback. More... | |
int32_t | ATCmdMqtt_setCallback (void *arg) |
Mqtt Client Set callback. More... | |
Controls MQTT Client programming options and capabilities.
int32_t ATCmdMqtt_connectCallback | ( | void * | arg | ) |
Mqtt Client Connect callback.
This routine connect to mqtt broker.
arg | - Points to command line buffer. |
Definition at line 577 of file atcmd_mqtt.c.
int32_t ATCmdMqtt_createCallback | ( | void * | arg | ) |
Mqtt Client Create callback.
This routine initialize the MQTT client instance.
arg | - Points to command line buffer. |
Definition at line 474 of file atcmd_mqtt.c.
int32_t ATCmdMqtt_deleteCallback | ( | void * | arg | ) |
Mqtt Client delete callback.
This routine delete mqtt client instance.
arg | - Points to command line buffer. |
Definition at line 546 of file atcmd_mqtt.c.
int32_t ATCmdMqtt_disconnectCallback | ( | void * | arg | ) |
Mqtt Client Disconnect callback.
This routine disconnect from mqtt broker.
arg | - Points to command line buffer. |
Definition at line 606 of file atcmd_mqtt.c.
int32_t ATCmdMqtt_publishCallback | ( | void * | arg | ) |
Mqtt Client Publish callback.
This routine send message to specific topic
arg | - Points to command line buffer. |
Definition at line 725 of file atcmd_mqtt.c.
int32_t ATCmdMqtt_setCallback | ( | void * | arg | ) |
Mqtt Client Set callback.
This routine set mqtt client configuration
arg | - Points to command line buffer. |
Definition at line 1142 of file atcmd_mqtt.c.
int32_t ATCmdMqtt_subscribeCallback | ( | void * | arg | ) |
Mqtt Client Subscribe callback.
This routine subscribe a topic for retrieving published messages
arg | - Points to command line buffer. |
Definition at line 850 of file atcmd_mqtt.c.
int32_t ATCmdMqtt_unsubscribeCallback | ( | void * | arg | ) |
Mqtt Client Unsubscribe callback.
This routine unsubscribe a topic
arg | - Points to command line buffer. |
Definition at line 968 of file atcmd_mqtt.c.