|
uint32_t | IpAddress |
|
uint32_t | SecuredConnection |
|
uint8_t | ServerName [MAX_SERVER_NAME] |
|
uint8_t | VendorToken [MAX_VENDOR_TOKEN_SIZE] |
|
Definition at line 73 of file ota.h.
§ IpAddress
Definition at line 75 of file ota.h.
§ SecuredConnection
uint32_t SecuredConnection |
Definition at line 76 of file ota.h.
§ ServerName
uint8_t ServerName[MAX_SERVER_NAME] |
Definition at line 77 of file ota.h.
§ VendorToken
uint8_t VendorToken[MAX_VENDOR_TOKEN_SIZE] |
Definition at line 78 of file ota.h.
The documentation for this struct was generated from the following file: