Network Services API  2.80.00.17
Data Fields
MQTTClient_SubscribeParams Struct Reference

#include <ti/net/mqtt/mqttclient.h>

Collaboration diagram for MQTTClient_SubscribeParams:
Collaboration graph

Data Fields

char * topic
 
MQTTClient_CallBack callback
 
uint8_t qos
 
uint8_t persistent
 

Field Documentation

§ topic

char* MQTTClient_SubscribeParams::topic

§ callback

MQTTClient_CallBack MQTTClient_SubscribeParams::callback

§ qos

uint8_t MQTTClient_SubscribeParams::qos

§ persistent

uint8_t MQTTClient_SubscribeParams::persistent

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale