Network Services API  2.80.00.17
Data Fields
MQTTClient_RecvMetaDataCB Struct Reference

#include <ti/net/mqtt/mqttclient.h>

Collaboration diagram for MQTTClient_RecvMetaDataCB:
Collaboration graph

Data Fields

const char * topic
 
int32_t topLen
 
bool dup
 
uint8_t qos
 
bool retain
 

Field Documentation

§ topic

const char* MQTTClient_RecvMetaDataCB::topic

§ topLen

int32_t MQTTClient_RecvMetaDataCB::topLen

§ dup

bool MQTTClient_RecvMetaDataCB::dup

§ qos

uint8_t MQTTClient_RecvMetaDataCB::qos

§ retain

bool MQTTClient_RecvMetaDataCB::retain

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale