![]() |
![]() |
The definition of a SD function table that contains the required set of functions to control a specific SD driver implementation. More...
#include <SD.h>
The definition of a SD function table that contains the required set of functions to control a specific SD driver implementation.
SD_CloseFxn SD_FxnTable::closeFxn |
Function to close the specified peripheral
SD_ControlFxn SD_FxnTable::controlFxn |
Function to implementation specific control function
SD_getNumSectorsFxn SD_FxnTable::getNumSectorsFxn |
Function to return the total number of sectors on the SD card
SD_getSectorSizeFxn SD_FxnTable::getSectorSizeFxn |
Function to return the sector size used to address the SD card
SD_InitFxn SD_FxnTable::initFxn |
Function to initialize the given data object
SD_InitializeFxn SD_FxnTable::initializeFxn |
Function to initialize the SD card
SD_OpenFxn SD_FxnTable::openFxn |
Function to open the specified peripheral
SD_ReadFxn SD_FxnTable::readFxn |
Function to read from the SD card
SD_WriteFxn SD_FxnTable::writeFxn |
Function to write to the SD card