![]() |
![]() |
PWMTimerCC32XX Hardware attributes. More...
#include <PWMTimerCC32XX.h>
Data Fields | |
uint32_t | pwmPin |
PWMTimerCC32XX Hardware attributes.
The 'pwmPin' field identifies which physical pin to use for a particular PWM channel as well as the corresponding Timer resource used to source the PWM signal. The encoded pin identifier macros for initializing the 'pwmPin' field must be selected from the PWMTimerCC32XX_HWAttrs 'pwmPin' field options macros.
A sample structure is shown below:
uint32_t PWMTimerCC32XX_HWAttrsV2::pwmPin |
Pin to output PWM signal on (see PWMTimerCC32XX_HWAttrs 'pwmPin' field options)