![]() |
![]() |
![]() |
Macros | |
#define | NVS_STATUS_SUCCESS (0) |
Successful status code returned by: NVS_control(), NVS_read(), NVS_write(), NVS_erase(), or NVS_lock(). More... | |
#define | NVS_STATUS_ERROR (-1) |
Generic error status code returned by: NVS_control(), NVS_erase(), or NVS_write(),. More... | |
#define | NVS_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by NVS_control() for undefined command codes. More... | |
#define | NVS_STATUS_TIMEOUT (-3) |
An error status code returned by NVS_lock() More... | |
#define | NVS_STATUS_INV_OFFSET (-4) |
An error status code returned by NVS_read(), NVS_write(), or NVS_erase() More... | |
#define | NVS_STATUS_INV_ALIGNMENT (-5) |
An error status code. More... | |
#define | NVS_STATUS_INV_SIZE (-6) |
An error status code returned by NVS_erase() and NVS_write() More... | |
#define | NVS_STATUS_INV_WRITE (-7) |
An error status code returned by NVS_write() More... | |
#define | NVS_STATUS_VERIFYBUFFER (-8) |
An error status code returned by NVS_write() More... | |
NVS_STATUS_* macros are general status codes returned by NVS_control()
#define NVS_STATUS_SUCCESS (0) |
Successful status code returned by: NVS_control(), NVS_read(), NVS_write(), NVS_erase(), or NVS_lock().
APIs returns NVS_STATUS_SUCCESS if the API was executed successfully.
#define NVS_STATUS_ERROR (-1) |
Generic error status code returned by: NVS_control(), NVS_erase(), or NVS_write(),.
APIs return NVS_STATUS_ERROR if the API was not executed successfully.
#define NVS_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by NVS_control() for undefined command codes.
NVS_control() returns NVS_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
#define NVS_STATUS_TIMEOUT (-3) |
An error status code returned by NVS_lock()
NVS_lock() will return this value if the timeout
has expired
#define NVS_STATUS_INV_OFFSET (-4) |
An error status code returned by NVS_read(), NVS_write(), or NVS_erase()
Error status code returned if the offset
argument is invalid (e.g., when offset + bufferSize exceeds the size of the region).
#define NVS_STATUS_INV_ALIGNMENT (-5) |
An error status code.
Error status code returned by NVS_erase() if the offset
argument is not aligned on a flash sector address.
#define NVS_STATUS_INV_SIZE (-6) |
An error status code returned by NVS_erase() and NVS_write()
Error status code returned by NVS_erase() if the size
argument is not a multiple of the flash sector size, or if offset
+ size
extends past the end of the region.
#define NVS_STATUS_INV_WRITE (-7) |
An error status code returned by NVS_write()
NVS_write() will return this value if NVS_WRITE_PRE_VERIFY is requested and a flash location can not be changed to the value desired.
#define NVS_STATUS_VERIFYBUFFER (-8) |
An error status code returned by NVS_write()
NVS_write() will return this value if NVS_WRITE_PRE_VERIFY or NVS_WRITE_POST_VERIFY is requested but the verification buffer has not been configured.