![]() |
![]() |
Macros | |
#define | I2C_STATUS_QUEUED (1) |
I2C transaction is queued but has not started. More... | |
#define | I2C_STATUS_SUCCESS (0) |
Successful status code returned by I2C API. More... | |
#define | I2C_STATUS_ERROR (-1) |
Generic error status code returned by I2C API. More... | |
#define | I2C_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by I2C_control() for undefined command codes. More... | |
#define | I2C_STATUS_TIMEOUT (-3) |
I2C operation timed-out. More... | |
#define | I2C_STATUS_CLOCK_TIMEOUT (-4) |
I2C serial clock line timeout. More... | |
#define | I2C_STATUS_ADDR_NACK (-5) |
I2C slave address not acknowledged. More... | |
#define | I2C_STATUS_DATA_NACK (-6) |
I2C data byte not acknowledged. More... | |
#define | I2C_STATUS_ARB_LOST (-7) |
I2C multi-master arbitration lost. More... | |
#define | I2C_STATUS_INCOMPLETE (-8) |
I2C transaction is in progress or returned without completing. More... | |
#define | I2C_STATUS_BUS_BUSY (-9) |
I2C bus already in use by another controller. The I2C transaction was therefore unable to start. More... | |
#define | I2C_STATUS_CANCEL (-10) |
I2C transaction canceled by I2C_cancel() More... | |
#define | I2C_STATUS_INVALID_TRANS (-11) |
I2C transaction is invalid. This may occur if: More... | |
These macros are reservations for I2C.h
I2CCC32XX_STATUS_* macros are command codes only defined in the I2CCC32XX.h driver implementation and need to:
#define I2C_STATUS_QUEUED (1) |
I2C transaction is queued but has not started.
#define I2C_STATUS_SUCCESS (0) |
Successful status code returned by I2C API.
#define I2C_STATUS_ERROR (-1) |
Generic error status code returned by I2C API.
#define I2C_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by I2C_control() for undefined command codes.
#define I2C_STATUS_TIMEOUT (-3) |
I2C operation timed-out.
#define I2C_STATUS_CLOCK_TIMEOUT (-4) |
I2C serial clock line timeout.
#define I2C_STATUS_ADDR_NACK (-5) |
I2C slave address not acknowledged.
#define I2C_STATUS_DATA_NACK (-6) |
I2C data byte not acknowledged.
#define I2C_STATUS_ARB_LOST (-7) |
I2C multi-master arbitration lost.
#define I2C_STATUS_INCOMPLETE (-8) |
I2C transaction is in progress or returned without completing.
#define I2C_STATUS_BUS_BUSY (-9) |
I2C bus already in use by another controller. The I2C transaction was therefore unable to start.
#define I2C_STATUS_CANCEL (-10) |
I2C transaction canceled by I2C_cancel()
#define I2C_STATUS_INVALID_TRANS (-11) |
I2C transaction is invalid. This may occur if: