![]() |
![]() |
Camera driver interface.
The Camera header file should be included in an application as follows:
The Camera driver is used to retrieve the data being transferred by the Camera sensor. This driver provides an API for capturing the image from the Camera sensor. The camera sensor control and implementation are the responsibility of the application using the interface.
The Camera driver has been designed to operate in an RTOS environment. It protects its transactions with OS primitives supplied by the underlying RTOS.
The Camera driver includes the following APIs:
In order to use the Camera APIs, the application is required to provide device-specific Camera configuration in the Board.c file. The Camera driver interface defines a configuration data structure:
The application must declare an array of Camera_Config elements, named Camera_config[]. Each element of Camera_config[] must be populated with pointers to a device specific Camera driver implementation's function table, driver object, and hardware attributes. The hardware attributes define properties such as the Camera peripheral's base address. Each element in Camera_config[] corresponds to a Camera instance, and none of the elements should have NULL pointers. There is no correlation between the index and the peripheral designation (such as Camera0 or Camera1). For example, it is possible to use Camera_config[0] for Camera1.
Because the Camera configuration is very device dependent, you will need to check the doxygen for the device specific Camera implementation. There you will find a description of the Camera hardware attributes. Please also refer to the Board.c file of any of your examples to see the Camera configuration.
The application initializes the Camera driver by calling Camera_init(). This function must be called before any other Camera API. Camera_init() iterates through the elements of the Camera_config[] array, calling the element's device implementation Camera initialization function.
The Camera_Params structure is passed to Camera_open(). If NULL is passed for the parameters, Camera_open() uses default parameters. A Camera_Params structure is initialized with default values by passing it to Camera_Params_init(). Some of the Camera parameters are described below. To see brief descriptions of all the parameters, see Camera_Params.
The Camera driver operates in either blocking mode or callback mode:
The capture mode is determined by the Camera_Params.captureMode parameter passed to Camera_open(). The Camera driver defaults to blocking mode, if the application does not set it.
Once a Camera driver instance is opened, the only way to change the capture mode is to close and re-open the Camera instance with the new capture mode.
The following example opens a Camera driver instance in blocking mode:
The following code example captures a frame.
This module serves as the main interface for RTOS applications. Its purpose is to redirect the module's APIs to specific peripheral implementations which are specified using a pointer to a Camera_FxnTable.
The Camera driver interface module is joined (at link time) to an array of Camera_Config data structures named Camera_config. Camera_config is implemented in the application with each entry being an instance of a Camera peripheral. Each entry in Camera_config contains a:
#include <stdint.h>#include <stddef.h>

Go to the source code of this file.
Data Structures | |
| struct | Camera_Params |
| Camera Parameters. More... | |
| struct | Camera_FxnTable |
| The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation. More... | |
| struct | Camera_Config_ |
| Camera Global configuration. More... | |
Macros | |
| #define | CAMERA_CMD_RESERVED (32) |
| #define | CAMERA_STATUS_RESERVED (-32) |
| #define | CAMERA_STATUS_SUCCESS (0) |
| Successful status code returned by Camera_control(). More... | |
| #define | CAMERA_STATUS_ERROR (-1) |
| Generic error status code returned by Camera_control(). More... | |
| #define | CAMERA_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by Camera_control() for undefined command codes. More... | |
| #define | Camera_WAIT_FOREVER (~(0U)) |
| Wait forever define. More... | |
Typedefs | |
| typedef struct Camera_Config_ * | Camera_Handle |
| A handle that is returned from a Camera_open() call. More... | |
| typedef void(* | Camera_Callback) (Camera_Handle handle, void *buf, size_t frameLength) |
| The definition of a callback function used by the Camera driver when used in Camera_MODE_CALLBACK. More... | |
| typedef void(* | Camera_CloseFxn) (Camera_Handle handle) |
| A function pointer to a driver specific implementation of Camera_close(). More... | |
| typedef int_fast16_t(* | Camera_ControlFxn) (Camera_Handle handle, uint_fast16_t cmd, void *arg) |
| A function pointer to a driver specific implementation of Camera_control(). More... | |
| typedef void(* | Camera_InitFxn) (Camera_Handle handle) |
| A function pointer to a driver specific implementation of Camera_init(). More... | |
| typedef Camera_Handle(* | Camera_OpenFxn) (Camera_Handle handle, Camera_Params *params) |
| A function pointer to a driver specific implementation of Camera_open(). More... | |
| typedef int_fast16_t(* | Camera_CaptureFxn) (Camera_Handle handle, void *buffer, size_t bufferlen, size_t *frameLen) |
| A function pointer to a driver specific implementation of Camera_capture(). More... | |
| typedef struct Camera_Config_ | Camera_Config |
| Camera Global configuration. More... | |
Functions | |
| void | Camera_close (Camera_Handle handle) |
| Function to close a Camera peripheral specified by the Camera handle. More... | |
| int_fast16_t | Camera_control (Camera_Handle handle, uint_fast16_t cmd, void *arg) |
| Function performs implementation specific features on a given Camera_Handle. More... | |
| void | Camera_init (void) |
| Function to initializes the Camera module. More... | |
| Camera_Handle | Camera_open (uint_least8_t index, Camera_Params *params) |
| Function to initialize a given Camera peripheral specified by the particular index value. The parameter specifies which mode the Camera will operate. More... | |
| void | Camera_Params_init (Camera_Params *params) |
| Function to initialize the Camera_Params structure to its defaults. More... | |
| int_fast16_t | Camera_capture (Camera_Handle handle, void *buffer, size_t bufferlen, size_t *frameLen) |
| Function that handles the Camera capture of a frame. More... | |
| #define Camera_WAIT_FOREVER (~(0U)) |
Wait forever define.
| typedef struct Camera_Config_* Camera_Handle |
A handle that is returned from a Camera_open() call.
| typedef void(* Camera_Callback) (Camera_Handle handle, void *buf, size_t frameLength) |
The definition of a callback function used by the Camera driver when used in Camera_MODE_CALLBACK.
| Camera_Handle | Camera_Handle |
| buf | Pointer to capture buffer |
| frameLength | length of frame |
| typedef void(* Camera_CloseFxn) (Camera_Handle handle) |
A function pointer to a driver specific implementation of Camera_close().
| typedef int_fast16_t(* Camera_ControlFxn) (Camera_Handle handle, uint_fast16_t cmd, void *arg) |
A function pointer to a driver specific implementation of Camera_control().
| typedef void(* Camera_InitFxn) (Camera_Handle handle) |
A function pointer to a driver specific implementation of Camera_init().
| typedef Camera_Handle(* Camera_OpenFxn) (Camera_Handle handle, Camera_Params *params) |
A function pointer to a driver specific implementation of Camera_open().
| typedef int_fast16_t(* Camera_CaptureFxn) (Camera_Handle handle, void *buffer, size_t bufferlen, size_t *frameLen) |
A function pointer to a driver specific implementation of Camera_capture().
| typedef struct Camera_Config_ Camera_Config |
Camera Global configuration.
The Camera_Config structure contains a set of pointers used to characterize the Camera driver implementation.
This structure needs to be defined before calling Camera_init() and it must not be changed thereafter.
| enum Camera_CaptureMode |
Camera capture mode settings.
This enum defines the capture mode for the configured Camera.
| enum Camera_HSyncPolarity |
| enum Camera_VSyncPolarity |
| enum Camera_ByteOrder |
| void Camera_close | ( | Camera_Handle | handle | ) |
Function to close a Camera peripheral specified by the Camera handle.
| handle | A Camera_Handle returned from Camera_open |
| int_fast16_t Camera_control | ( | Camera_Handle | handle, |
| uint_fast16_t | cmd, | ||
| void * | arg | ||
| ) |
Function performs implementation specific features on a given Camera_Handle.
Commands for Camera_control can originate from Camera.h or from implementation specific Camera*.h (CameraCC32XX.h, etc.. ) files. While commands from Camera.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific Camera*.h files add unique driver capabilities but are not API portable across all Camera driver implementations.
Commands supported by Camera.h follow a Camera_CMD_<cmd> naming convention.
Commands supported by Camera*.h follow a Camera*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.
See Camera_control command codes for command codes.
See Camera_control return status codes for status codes.
| handle | A Camera handle returned from Camera_open() |
| cmd | Camera.h or Camera*.h commands. |
| arg | An optional R/W (read/write) command argument accompanied with cmd |
| void Camera_init | ( | void | ) |
Function to initializes the Camera module.
| Camera_Handle Camera_open | ( | uint_least8_t | index, |
| Camera_Params * | params | ||
| ) |
Function to initialize a given Camera peripheral specified by the particular index value. The parameter specifies which mode the Camera will operate.
| index | Logical peripheral number for the Camera indexed into the Camera_config table |
| params | Pointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only). |
| void Camera_Params_init | ( | Camera_Params * | params | ) |
Function to initialize the Camera_Params structure to its defaults.
| params | An pointer to Camera_Params structure for initialization |
Defaults values are: captureMode = Camera_MODE_BLOCKING; outputClock = 24000000; hsyncPolarity = Camera_HSYNC_POLARITY_HIGH; vsyncPolarity = Camera_VSYNC_POLARITY_HIGH; pixelClkConfig = Camera_PCLK_CONFIG_RISING_EDGE; byteOrder = Camera_BYTE_ORDER_NORMAL; interfaceSync = Camera_INTERFACE_SYNC_ON; stopConfig = Camera_STOP_CAPTURE_FRAME_END; startConfig = Camera_START_CAPTURE_FRAME_START; captureTimeout = Camera_WAIT_FOREVER; captureCallback = NULL;
| int_fast16_t Camera_capture | ( | Camera_Handle | handle, |
| void * | buffer, | ||
| size_t | bufferlen, | ||
| size_t * | frameLen | ||
| ) |
Function that handles the Camera capture of a frame.
In Camera_MODE_BLOCKING, Camera_capture will block task execution until the capture is complete.
In Camera_MODE_CALLBACK, Camera_capture does not block task execution and calls a callback function specified by captureCallbackFxn. The Camera buffer must stay persistent until the Camera_capture function has completed!
| handle | A Camera_Handle |
| buffer | A pointer to a WO (write-only) buffer into which the captured frame is placed |
| bufferlen | Length (in bytes) of the capture buffer |
| frameLen | Pointer to return number of bytes captured. |