GPIO pin identification macros used to configure GPIO pins

Device specific GPIO port/pin identifiers to be used within the board's GPIO_PinConfig table.

#define GPIOCC32XX_EMPTY_PIN
 
#define GPIOCC32XX_GPIO_00   0x0001
 
#define GPIOCC32XX_GPIO_01   0x0002
 
#define GPIOCC32XX_GPIO_02   0x0004
 
#define GPIOCC32XX_GPIO_03   0x0008
 
#define GPIOCC32XX_GPIO_04   0x0010
 
#define GPIOCC32XX_GPIO_05   0x0020
 
#define GPIOCC32XX_GPIO_06   0x0040
 
#define GPIOCC32XX_GPIO_07   0x0080
 
#define GPIOCC32XX_GPIO_08   0x0101
 
#define GPIOCC32XX_GPIO_09   0x0102
 
#define GPIOCC32XX_GPIO_10   0x0104
 
#define GPIOCC32XX_GPIO_11   0x0108
 
#define GPIOCC32XX_GPIO_12   0x0110
 
#define GPIOCC32XX_GPIO_13   0x0120
 
#define GPIOCC32XX_GPIO_14   0x0140
 
#define GPIOCC32XX_GPIO_15   0x0180
 
#define GPIOCC32XX_GPIO_16   0x0201
 
#define GPIOCC32XX_GPIO_17   0x0202
 
#define GPIOCC32XX_GPIO_22   0x0240
 
#define GPIOCC32XX_GPIO_23   0x0280
 
#define GPIOCC32XX_GPIO_24   0x0301
 
#define GPIOCC32XX_GPIO_25   0x0302
 
#define GPIOCC32XX_GPIO_26   0x0304
 
#define GPIOCC32XX_GPIO_27   0x0308
 
#define GPIOCC32XX_GPIO_28   0x0310
 
#define GPIOCC32XX_GPIO_29   0x0320
 
#define GPIOCC32XX_GPIO_30   0x0340
 
#define GPIOCC32XX_GPIO_31   0x0380
 
#define GPIOCC32XX_GPIO_32   0x0401
 

CC32xx device specific GPIO_PinConfig macros

#define GPIOCC32XX_USE_STATIC
 

Detailed Description

Macro Definition Documentation

§ GPIOCC32XX_EMPTY_PIN

#define GPIOCC32XX_EMPTY_PIN

§ GPIOCC32XX_GPIO_00

#define GPIOCC32XX_GPIO_00   0x0001

PIN 50

§ GPIOCC32XX_GPIO_01

#define GPIOCC32XX_GPIO_01   0x0002

PIN 55

§ GPIOCC32XX_GPIO_02

#define GPIOCC32XX_GPIO_02   0x0004

PIN 57

§ GPIOCC32XX_GPIO_03

#define GPIOCC32XX_GPIO_03   0x0008

PIN 58

§ GPIOCC32XX_GPIO_04

#define GPIOCC32XX_GPIO_04   0x0010

PIN 59

§ GPIOCC32XX_GPIO_05

#define GPIOCC32XX_GPIO_05   0x0020

PIN 60

§ GPIOCC32XX_GPIO_06

#define GPIOCC32XX_GPIO_06   0x0040

PIN 61

§ GPIOCC32XX_GPIO_07

#define GPIOCC32XX_GPIO_07   0x0080

PIN 62

§ GPIOCC32XX_GPIO_08

#define GPIOCC32XX_GPIO_08   0x0101

PIN 63

§ GPIOCC32XX_GPIO_09

#define GPIOCC32XX_GPIO_09   0x0102

PIN 64

§ GPIOCC32XX_GPIO_10

#define GPIOCC32XX_GPIO_10   0x0104

PIN 1

§ GPIOCC32XX_GPIO_11

#define GPIOCC32XX_GPIO_11   0x0108

PIN 2

§ GPIOCC32XX_GPIO_12

#define GPIOCC32XX_GPIO_12   0x0110

PIN 3

§ GPIOCC32XX_GPIO_13

#define GPIOCC32XX_GPIO_13   0x0120

PIN 4

§ GPIOCC32XX_GPIO_14

#define GPIOCC32XX_GPIO_14   0x0140

PIN 5

§ GPIOCC32XX_GPIO_15

#define GPIOCC32XX_GPIO_15   0x0180

PIN 6

§ GPIOCC32XX_GPIO_16

#define GPIOCC32XX_GPIO_16   0x0201

PIN 7

§ GPIOCC32XX_GPIO_17

#define GPIOCC32XX_GPIO_17   0x0202

PIN 8

§ GPIOCC32XX_GPIO_22

#define GPIOCC32XX_GPIO_22   0x0240

PIN 15

§ GPIOCC32XX_GPIO_23

#define GPIOCC32XX_GPIO_23   0x0280

PIN 16

§ GPIOCC32XX_GPIO_24

#define GPIOCC32XX_GPIO_24   0x0301

PIN 17

§ GPIOCC32XX_GPIO_25

#define GPIOCC32XX_GPIO_25   0x0302

PIN 21

§ GPIOCC32XX_GPIO_26

#define GPIOCC32XX_GPIO_26   0x0304

PIN 29

§ GPIOCC32XX_GPIO_27

#define GPIOCC32XX_GPIO_27   0x0308

PIN 30

§ GPIOCC32XX_GPIO_28

#define GPIOCC32XX_GPIO_28   0x0310

PIN 18

§ GPIOCC32XX_GPIO_29

#define GPIOCC32XX_GPIO_29   0x0320

PIN 20

§ GPIOCC32XX_GPIO_30

#define GPIOCC32XX_GPIO_30   0x0340

PIN 53

§ GPIOCC32XX_GPIO_31

#define GPIOCC32XX_GPIO_31   0x0380

PIN 45

§ GPIOCC32XX_GPIO_32

#define GPIOCC32XX_GPIO_32   0x0401

PIN 52

§ GPIOCC32XX_USE_STATIC

#define GPIOCC32XX_USE_STATIC

use statically-defined parking state

© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale