![]() |
SimpleLink CC31xx/CC32xx Host Driver
Version 3.0.1.70
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u8 | TokenValueLen |
_u8 | TokenNameLen |
_u8 | TokenName [SL_NETAPP_MAX_TOKEN_NAME_LEN] |
_u16 | Padd |
Definition at line 971 of file protocol.h.
_u16 Padd |
Definition at line 976 of file protocol.h.
_u8 TokenName[SL_NETAPP_MAX_TOKEN_NAME_LEN] |
Definition at line 975 of file protocol.h.
_u8 TokenNameLen |
Definition at line 974 of file protocol.h.
_u8 TokenValueLen |
Definition at line 973 of file protocol.h.