![]() |
SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
|
Definition at line 85 of file OtaArchive.h.
uint32_t Bundle |
Definition at line 94 of file OtaArchive.h.
uint8_t CertificateFileNameBuf[MAX_FILE_NAME_SIZE] |
Definition at line 88 of file OtaArchive.h.
uint8_t FileNameBuf[MAX_FILE_NAME_SIZE] |
Definition at line 87 of file OtaArchive.h.
uint8_t SavedInFS |
Definition at line 95 of file OtaArchive.h.
uint32_t Secured |
Definition at line 93 of file OtaArchive.h.
uint8_t Sha256Digest[MAX_SHA256_DIGEST_SIZE] |
Definition at line 91 of file OtaArchive.h.
uint16_t Sha256DigestLen |
Definition at line 92 of file OtaArchive.h.
uint8_t SignatureBuf[MAX_SIGNATURE_SIZE] |
Definition at line 89 of file OtaArchive.h.
uint32_t SignatureLen |
Definition at line 90 of file OtaArchive.h.