Network Services API
2.80.00.17
|
Global parameters and attributes used to establish connections. More...
#include <ti/net/slnetconn.h>
Data Fields | |
uint32_t | ifBitmap |
char * | pServerAddress |
uint16_t | serverAddrFamily |
Global parameters and attributes used to establish connections.
This structure is set using the SlNetConn_setConfiguration(). If the function is not called the default values will apply.
uint32_t SlNetConn_config_t::ifBitmap |
bitmask of SlNet interfaces that will be used to establish the connection. The bit corresponds to the I/F ID as defined when using SlNetIf_add(). Default is 0 (which means all available interfaces).
char* SlNetConn_config_t::pServerAddress |
IP address of a global server used to verify the internet connection. Default is "8.8.8.8" (google DNS server).
uint16_t SlNetConn_config_t::serverAddrFamily |
global server address family: