![]() |
SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
|
Data Fields | |
uint8_t | FileNameBuf [MAX_FILE_NAME_SIZE] |
uint8_t * | pFileName |
uint32_t | FileSize |
int16_t | FileType |
uint32_t | ulToken |
int32_t | lFileHandle |
uint32_t | WriteFileOffset |
Definition at line 106 of file OtaArchive.h.
uint8_t FileNameBuf[MAX_FILE_NAME_SIZE] |
Definition at line 109 of file OtaArchive.h.
uint32_t FileSize |
Definition at line 111 of file OtaArchive.h.
int16_t FileType |
Definition at line 112 of file OtaArchive.h.
int32_t lFileHandle |
Definition at line 115 of file OtaArchive.h.
uint8_t* pFileName |
Definition at line 110 of file OtaArchive.h.
uint32_t ulToken |
Definition at line 114 of file OtaArchive.h.
uint32_t WriteFileOffset |
Definition at line 116 of file OtaArchive.h.