![]() |
SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
|
Data Fields | |
int16_t | NumFiles |
int16_t | NumFilesSavedInFS |
OtaArchive_BundleFileInfo_t | BundleFileInfo [MAX_BUNDLE_CMD_FILES] |
uint8_t | VerifiedSignature |
uint16_t | TotalParsedBytes |
Definition at line 97 of file OtaArchive.h.
OtaArchive_BundleFileInfo_t BundleFileInfo[MAX_BUNDLE_CMD_FILES] |
Definition at line 101 of file OtaArchive.h.
int16_t NumFiles |
Definition at line 99 of file OtaArchive.h.
int16_t NumFilesSavedInFS |
Definition at line 100 of file OtaArchive.h.
uint16_t TotalParsedBytes |
Definition at line 103 of file OtaArchive.h.
uint8_t VerifiedSignature |
Definition at line 102 of file OtaArchive.h.