SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
OTA_memBlock Struct Reference

Data Fields

uint8_t Buff [OTA_BLOCK_SIZE]
 

Detailed Description

Definition at line 54 of file ota.h.

Field Documentation

§ Buff

uint8_t Buff[OTA_BLOCK_SIZE]

Definition at line 56 of file ota.h.


The documentation for this struct was generated from the following file: