SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.65
Simplifies the implementation of Internet connectivity
SlNetCfgSetGet_t Struct Reference

Data Fields

_u16 Status
 
_u16 ConfigId
 
_u16 ConfigOpt
 
_u16 ConfigLen
 

Detailed Description

Definition at line 751 of file protocol.h.

Field Documentation

§ ConfigId

_u16 ConfigId

Definition at line 754 of file protocol.h.

§ ConfigLen

_u16 ConfigLen

Definition at line 756 of file protocol.h.

§ ConfigOpt

_u16 ConfigOpt

Definition at line 755 of file protocol.h.

§ Status

_u16 Status

Definition at line 753 of file protocol.h.


The documentation for this struct was generated from the following file: