SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
|
Data Fields | |
Ota_optServerInfo * | pOtaServerInfo |
int32_t | CurrDirFileIndex |
OtaDirData_t | OtaDirData |
int16_t | ServerSockId |
int32_t | PortNum |
int16_t | FileSockId |
uint8_t * | pRecvChunk |
uint8_t * | pNetBuf |
Definition at line 54 of file CdnClient.h.
int32_t CurrDirFileIndex |
Definition at line 60 of file CdnClient.h.
int16_t FileSockId |
Definition at line 66 of file CdnClient.h.
OtaDirData_t OtaDirData |
Definition at line 61 of file CdnClient.h.
uint8_t* pNetBuf |
Definition at line 68 of file CdnClient.h.
int32_t PortNum |
Definition at line 65 of file CdnClient.h.
Ota_optServerInfo* pOtaServerInfo |
Definition at line 57 of file CdnClient.h.
uint8_t* pRecvChunk |
Definition at line 67 of file CdnClient.h.
int16_t ServerSockId |
Definition at line 64 of file CdnClient.h.