Data Fields
CameraCC32XXDMA_Object Struct Reference

CameraCC32XXDMA Object. More...

#include <CameraCC32XXDMA.h>

Collaboration diagram for CameraCC32XXDMA_Object:
Collaboration graph
[legend]

Data Fields

bool opened
 
Camera_CaptureMode operationMode
 
Camera_Callback captureCallback
 
uint32_t captureTimeout
 
void * captureBuf
 
size_t bufferlength
 
size_t frameLength
 
bool cameraDMA_PingPongMode
 
size_t cameraDMAxIntrRcvd
 
bool inUse
 
SemaphoreP_Handle captureSem
 
HwiP_Handle hwiHandle
 

Detailed Description

CameraCC32XXDMA Object.

The application must not access any member variables of this structure!

Field Documentation

§ opened

bool CameraCC32XXDMA_Object::opened

§ operationMode

Camera_CaptureMode CameraCC32XXDMA_Object::operationMode

§ captureCallback

Camera_Callback CameraCC32XXDMA_Object::captureCallback

§ captureTimeout

uint32_t CameraCC32XXDMA_Object::captureTimeout

§ captureBuf

void* CameraCC32XXDMA_Object::captureBuf

§ bufferlength

size_t CameraCC32XXDMA_Object::bufferlength

§ frameLength

size_t CameraCC32XXDMA_Object::frameLength

§ cameraDMA_PingPongMode

bool CameraCC32XXDMA_Object::cameraDMA_PingPongMode

§ cameraDMAxIntrRcvd

size_t CameraCC32XXDMA_Object::cameraDMAxIntrRcvd

§ inUse

bool CameraCC32XXDMA_Object::inUse

§ captureSem

SemaphoreP_Handle CameraCC32XXDMA_Object::captureSem

§ hwiHandle

HwiP_Handle CameraCC32XXDMA_Object::hwiHandle

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale