Data Fields
Camera_Config_ Struct Reference

Camera Global configuration. More...

#include <Camera.h>

Collaboration diagram for Camera_Config_:
Collaboration graph
[legend]

Data Fields

Camera_FxnTable const * fxnTablePtr
 
void * object
 
void const * hwAttrs
 

Detailed Description

Camera Global configuration.

The Camera_Config structure contains a set of pointers used to characterize the Camera driver implementation.

This structure needs to be defined before calling Camera_init() and it must not be changed thereafter.

See also
Camera_init()

Field Documentation

§ fxnTablePtr

Camera_FxnTable const* Camera_Config_::fxnTablePtr

Pointer to a table of driver-specific implementations of Camera APIs

§ object

void* Camera_Config_::object

Pointer to a driver specific data object

§ hwAttrs

void const* Camera_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale