60 #ifndef ti_drivers_uart_UARTCC32XXDMA__include 61 #define ti_drivers_uart_UARTCC32XXDMA__include 66 #include <ti/drivers/dpl/ClockP.h> 67 #include <ti/drivers/dpl/HwiP.h> 69 #include <ti/drivers/dpl/SemaphoreP.h> 85 #define UARTCC32XXDMA_PIN_UNASSIGNED 0xFFF 96 #define UARTCC32XXDMA_PIN_01_UART1_TX 0x700 97 #define UARTCC32XXDMA_PIN_02_UART1_RX 0x701 98 #define UARTCC32XXDMA_PIN_03_UART0_TX 0x702 99 #define UARTCC32XXDMA_PIN_04_UART0_RX 0x703 100 #define UARTCC32XXDMA_PIN_07_UART1_TX 0x506 101 #define UARTCC32XXDMA_PIN_08_UART1_RX 0x507 102 #define UARTCC32XXDMA_PIN_16_UART1_TX 0x20F 103 #define UARTCC32XXDMA_PIN_17_UART1_RX 0x210 104 #define UARTCC32XXDMA_PIN_45_UART0_RX 0x92C 105 #define UARTCC32XXDMA_PIN_45_UART1_RX 0x22C 106 #define UARTCC32XXDMA_PIN_53_UART0_TX 0x934 107 #define UARTCC32XXDMA_PIN_55_UART0_TX 0x336 108 #define UARTCC32XXDMA_PIN_55_UART1_TX 0x636 109 #define UARTCC32XXDMA_PIN_57_UART0_RX 0x338 110 #define UARTCC32XXDMA_PIN_57_UART1_RX 0x638 111 #define UARTCC32XXDMA_PIN_58_UART1_TX 0x639 112 #define UARTCC32XXDMA_PIN_59_UART1_RX 0x63A 113 #define UARTCC32XXDMA_PIN_62_UART0_TX 0xB3D 118 #define UARTCC32XXDMA_PIN_50_UART0_CTS 0xC31 119 #define UARTCC32XXDMA_PIN_50_UART0_RTS 0x331 120 #define UARTCC32XXDMA_PIN_50_UART1_RTS 0xA31 121 #define UARTCC32XXDMA_PIN_52_UART0_RTS 0x633 122 #define UARTCC32XXDMA_PIN_61_UART0_RTS 0x53C 123 #define UARTCC32XXDMA_PIN_61_UART0_CTS 0x63C 124 #define UARTCC32XXDMA_PIN_61_UART1_CTS 0x33C 125 #define UARTCC32XXDMA_PIN_62_UART0_RTS 0xA3D 126 #define UARTCC32XXDMA_PIN_62_UART1_RTS 0x33D 131 #define UARTCC32XXDMA_FLOWCTRL_NONE 0 136 #define UARTCC32XXDMA_FLOWCTRL_HARDWARE 1 170 #define UARTCC32XXDMA_CMD_IS_BUSY (UART_CMD_RESERVED + 0) 181 #define UARTCC32XXDMA_CMD_IS_RX_DATA_AVAILABLE (UART_CMD_RESERVED + 1) 192 #define UARTCC32XXDMA_CMD_IS_TX_SPACE_AVAILABLE (UART_CMD_RESERVED + 2) UARTCC32XXDMA Hardware attributes.
Definition: UARTCC32XXDMA.h:265
UART_STOP
UART stop bit settings.
Definition: UART.h:522
Power_NotifyObj postNotify
Definition: UARTCC32XXDMA.h:334
uint32_t flowControl
Definition: UARTCC32XXDMA.h:273
uint16_t rxPin
Definition: UARTCC32XXDMA.h:279
PowerCC32XX_ParkState prevParkTX
Definition: UARTCC32XXDMA.h:336
size_t readSize
Definition: UARTCC32XXDMA.h:324
UARTCC32XXDMA Object.
Definition: UARTCC32XXDMA.h:298
UART_Callback writeCallback
Definition: UARTCC32XXDMA.h:306
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:634
unsigned int writeTimeout
Definition: UARTCC32XXDMA.h:304
UART_PAR
UART parity type settings.
Definition: UART.h:532
UDMACC32XX_Handle dmaHandle
Definition: UARTCC32XXDMA.h:342
unsigned int baseAddr
Definition: UARTCC32XXDMA.h:267
const void * writeBuf
Definition: UARTCC32XXDMA.h:317
UART_Mode
UART mode settings.
Definition: UART.h:427
UART_Echo readEcho
Definition: UARTCC32XXDMA.h:314
UART_DataMode
UART data mode settings.
Definition: UART.h:482
size_t readCount
Definition: UARTCC32XXDMA.h:323
UART_ReturnMode
UART return mode settings.
Definition: UART.h:460
SemaphoreP_Handle readSem
Definition: UARTCC32XXDMA.h:328
unsigned int powerMgrId
Definition: UARTCC32XXDMA.h:335
UART_Echo
UART echo settings.
Definition: UART.h:500
uDMA driver implementation for CC32XX.
unsigned int intNum
Definition: UARTCC32XXDMA.h:269
UART Global configuration.
Definition: UART.h:677
SemaphoreP_Handle writeSem
Definition: UARTCC32XXDMA.h:327
uint16_t txPin
Definition: UARTCC32XXDMA.h:281
void * readBuf
Definition: UARTCC32XXDMA.h:322
UDMACC32XX Global configuration.
Definition: UDMACC32XX.h:125
uint16_t ctsPin
Definition: UARTCC32XXDMA.h:283
Power manager interface for the CC32XX.
ClockP_Handle txFifoEmptyClk
Definition: UARTCC32XXDMA.h:333
uint32_t baudRate
Definition: UARTCC32XXDMA.h:310
Power notify object structure.
Definition: Power.h:443
UART_PAR parityType
Definition: UARTCC32XXDMA.h:313
Universal Asynchronous Receiver-Transmitter (UART) Driver.
bool opened
Definition: UARTCC32XXDMA.h:300
UART_STOP stopBits
Definition: UARTCC32XXDMA.h:312
UART_LEN dataLength
Definition: UARTCC32XXDMA.h:311
UART_DataMode readDataMode
Definition: UARTCC32XXDMA.h:308
uint16_t rtsPin
Definition: UARTCC32XXDMA.h:339
uint16_t rtsPin
Definition: UARTCC32XXDMA.h:285
unsigned int readTimeout
Definition: UARTCC32XXDMA.h:303
size_t writeCount
Definition: UARTCC32XXDMA.h:318
size_t writeSize
Definition: UARTCC32XXDMA.h:319
UARTCC32XXDMA_ErrorCallback errorFxn
Definition: UARTCC32XXDMA.h:290
HwiP_Handle hwiHandle
Definition: UARTCC32XXDMA.h:330
void(* UARTCC32XXDMA_ErrorCallback)(UART_Handle handle, uint32_t error)
The definition of an optional callback function used by the UART driver to notify the application whe...
Definition: UARTCC32XXDMA.h:212
UART_LEN
UART data length settings.
Definition: UART.h:510
unsigned long rxChannelIndex
Definition: UARTCC32XXDMA.h:275
PowerCC32XX_ParkState prevParkRTS
Definition: UARTCC32XXDMA.h:338
uint16_t txPin
Definition: UARTCC32XXDMA.h:337
UART_Mode writeMode
Definition: UARTCC32XXDMA.h:302
UART_DataMode writeDataMode
Definition: UARTCC32XXDMA.h:309
struct UARTCC32XXDMA_Object * UARTCC32XXDMA_Handle
UART_Mode readMode
Definition: UARTCC32XXDMA.h:301
unsigned long txChannelIndex
Definition: UARTCC32XXDMA.h:277
unsigned int intPriority
Definition: UARTCC32XXDMA.h:271
UART_Callback readCallback
Definition: UARTCC32XXDMA.h:305
const UART_FxnTable UARTCC32XXDMA_fxnTable
UART_ReturnMode readReturnMode
Definition: UARTCC32XXDMA.h:307
void(* UART_Callback)(UART_Handle handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:420
PowerCC32XX_ParkState
Enumeration of states a pin can be parked in.
Definition: PowerCC32XX.h:385