Network Services API  2.75.00.17
Data Fields
_MQTTServer_SubscribeParams_ Struct Reference

#include <ti/net/mqtt/mqttserver.h>

Collaboration diagram for _MQTTServer_SubscribeParams_:
Collaboration graph

Data Fields

char * topic
 
MQTTServer_CallBack callback
 
uint8_t persistent
 

Field Documentation

§ topic

char* _MQTTServer_SubscribeParams_::topic

§ callback

MQTTServer_CallBack _MQTTServer_SubscribeParams_::callback

optional - if NULL use the default callback

§ persistent

uint8_t _MQTTServer_SubscribeParams_::persistent

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale