The HTTP server provides APIs to instantiate an HTTP server, and handle requests from HTTP clients.
More...
|
void | HTTPServer_init (void) |
| Initialize the HTTPServer module. More...
|
|
void | HTTPServer_Params_init (HTTPServer_Params *params) |
| Initialize the instance create params structure. More...
|
|
void | HTTPServer_enableSecurity (HTTPServer_Handle srv, SlNetSockSecAttrib_t *securityAttributes, bool beginSecurely) |
| Attach security params to the created, but not yet initialized server. More...
|
|
HTTPServer_Handle | HTTPServer_create (const URLHandler_Setup *urlh, int numURLh, HTTPServer_Params *params) |
| Create an HTTPServer instance. More...
|
|
void | HTTPServer_delete (HTTPServer_Handle *srv) |
| Delete an HTTPServer instance. More...
|
|
void | HTTPServer_sendSimpleResponse (int s, int status, const char *type, size_t len, const void *buf) |
| Send a simple, complete response to a client. More...
|
|
void | HTTPServer_sendResponse (int s, int status, const char *headers[], int numHeaders, size_t len, const void *buf) |
| Send a complete response to a client. More...
|
|
void | HTTPServer_sendErrorResponse (int s, int status) |
| Send an error response to a client. More...
|
|
void | HTTPServer_sendResponseChunked (int s, int status, const char *type) |
| Begin the process of sending a chunked response to a client. More...
|
|
void | HTTPServer_sendChunk (int s, const void *buf, size_t len) |
| Continue and complete the process of sending a chunked response to a client. More...
|
|
int | HTTPServer_serveSelect (HTTPServer_Handle srv, const struct sockaddr *addr, int len, int backlog) |
| Begin the HTTP Server's main processing loop. More...
|
|
bool | HTTPServer_stop (HTTPServer_Handle srv, uint32_t timeout) |
| Stop a currently running server. More...
|
|
bool | HTTPServer_isSessionSecure (URLHandler_Session sess) |
| Obtain the session's security status. More...
|
|
The HTTP server provides APIs to instantiate an HTTP server, and handle requests from HTTP clients.
Library Usage
To use the HTTPServer APIs, the application should include its header file as follows:
And, add the following HTTP library to the link line:
.../source/ti/net/http/{toolchain}/{isa}/httpserver_{profile}.a
§ HTTPServer_EACCEPTFAIL
#define HTTPServer_EACCEPTFAIL (-2) |
Internal accept() call failed.
§ HTTPServer_ESOCKETFAIL
#define HTTPServer_ESOCKETFAIL (-3) |
Internal network socket creation failure.
§ HTTPServer_EBINDFAIL
#define HTTPServer_EBINDFAIL (-4) |
Internal bind() call failed.
§ HTTPServer_ELISTENFAIL
#define HTTPServer_ELISTENFAIL (-5) |
Internal listen() call failed.
§ HTTPServer_EMEMFAIL
#define HTTPServer_EMEMFAIL (-6) |
Internal memory allocation or object creation failure.
§ HTTPServer_EMQFAIL
#define HTTPServer_EMQFAIL (-7) |
Internal mq creation failure.
§ HTTPServer_EMUTEXFAIL
#define HTTPServer_EMUTEXFAIL (-8) |
Internal mutex-related failure.
§ URLHandler_GET
§ URLHandler_POST
#define URLHandler_POST 2 |
§ URLHandler_PUT
§ URLHandler_PATCH
#define URLHandler_PATCH 4 |
§ URLHandler_DELETE
#define URLHandler_DELETE 5 |
§ URLHandler_ENOTHANDLED
#define URLHandler_ENOTHANDLED 0 |
§ URLHandler_EHANDLED
#define URLHandler_EHANDLED 1 |
§ URLHandler_EERRORHANDLED
#define URLHandler_EERRORHANDLED 2 |
§ URLHandler_EHANDLEDSTOP
#define URLHandler_EHANDLEDSTOP 3 |
§ HTTPServer_Params
HTTPServer instance create parameters.
§ HTTPServer_Handle
HTTPServer instance object handle.
§ URLHandler_Handle
A placeholder used to refer to a user-defined type.
This object handle is the type returned from the URLHandler_CreateFxn and passed to all other URLHandler_* functions.
§ URLHandler_Session
§ URLHandler_CreateFxn
Create a user-defined URLHandler_Object.
This function (if used) should be used to instantiate a user-defined URLHandler_Handle object that contains whatever information is deemed necessary to pass to other URLHandler_* functions while the server is running. The handle of the user-defined type should be cast as a URLHandler_Handle before returning it from this function. The handle is later passed to other URLHandler_* functions in order to access session-specific data. The handle should be recast as the user-defined type before accessing it in other URLHandler_* functions.
- Parameters
-
[in] | params | Optional parameters to specify characteristics |
[in] | session | Handler to current client session |
- Return values
-
URLHandler | instance handle |
- See also
- URLHandler_ProcessFxn()
-
URLHandler_ScanFieldFxn()
-
URLHandler_DeleteFxn()
§ URLHandler_ProcessFxn
typedef int(* URLHandler_ProcessFxn) (URLHandler_Handle u, int method, const char *url, const char *urlArgs, int contentLength, int s) |
Process an HTTP request.
This function is called after an HTTP request is received and the request headers have been processed, possibly by calling the URLHandler_ScanFieldFxn(). For every request received by the server this method is called once per URLHandler until a URLHandler handles the request.
The body of a request can be retrieved by calling recv() with the supplied socket s
argument. The length of the request body is available in the contentLength
parameter. Given the HTTP method, URL, and request body, this function can determine how to proceed. i.e. if a GET request is received, this is where the resource identified by the URL should be fetched; If a POST request is made, this is where the data passed within urlArgs
or the request body can be parsed and acted upon (i.e. stored within the server); etc.
After processing a request, this function should construct a response. This involves selecting a status code (see the HTTP_STATUS_CODE
enum in ti/net/http/http.h), creating any desired headers, and creating the response body.
Once the components of the response have been created, they can be sent to the client via the recommended HTTPServer_send* methods. Note that users can directly send a response using send(), however the user is then responsible for creating well-formed headers and responses.
The u
argument contains the URLHandler_Handle that was returned from URLHandler_CreateFxn(), or NULL if the handler didn't provide one.
The return value of this function determines how the server proceeds:
- If URLHandler_ENOTHANDLED is returned and there are more URLHandlers whose process methods have not been called, the server will proceed to call said process methods, one by one, until the request is handled or until there are no more URLHandler->process methods available.
- If URLHandler_ENOTHANDLED is returned and no URLHandlers are able to handle the request, a 404 response will be sent to the client.
- If URLHandler_EHANDLEDSTOP is returned, the server will remove all open sessions, close its listening socket, and shut down.
- If URLHandler_EERRORHANDLED is returned, the current session (client connection) is closed and the server continues.
- Parameters
-
[in] | u | Handle to the URL Handler containing relevant data |
[in] | method | HTTP method of the request being parsed |
[in] | url | URI of the current request |
[in] | urlArgs | The query string, if present |
[in] | contentLength | Content-Length (body length) header value, if present |
[in] | s | TCP/IP socket connected to a client |
- Return values
-
- See also
- HTTPServer_sendSimpleResponse()
-
URLHandler_ScanFieldFxn()
§ URLHandler_ScanFieldFxn
typedef void(* URLHandler_ScanFieldFxn) (URLHandler_Handle u, int method, const char *url, const char *field) |
Scan for specific request headers.
This function can be used to process headers of incoming requests. Every URL Handler with this function defined will have each header passed into this function, one by one. It is called when a request is received by the server, before the request is sent to the URLHandler_ProcessFxn. The Content-Length header is parsed automatically by the server (however, it will still be passed into this function, should the developer want to examine it).
- Parameters
-
[in] | u | Handle to the URL Handler containing relevant data |
[in] | method | HTTP method of the request being parsed |
[in] | url | URI of the current request |
[in] | field | Specific request line containing the header |
- See also
- URLHandler_ProcessFxn()
§ URLHandler_DeleteFxn
Delete a URLHandler.
This function is called when the session associated with the handler parameter is closed. Any memory allocated for the URLHandler (i.e. in the _create function) should be cleaned up here.
- Parameters
-
[in] | u | The Handler for deletion |
- See also
- URLHandler_CreateFxn()
§ URLHandler_Setup
Structure containing URL Handler components.
This structure contains parameters needed for setup of a user- defined URLHandler object and pointers to associated user-defined URLHandler_* functions. The created HTTP Server maintains a table of this data structure for each unique URL Handler.
§ HTTPServer_init()
void HTTPServer_init |
( |
void |
| ) |
|
Initialize the HTTPServer module.
§ HTTPServer_Params_init()
Initialize the instance create params structure.
- Parameters
-
[in] | params | params structure to initialize |
§ HTTPServer_enableSecurity()
Attach security params to the created, but not yet initialized server.
- Parameters
-
[in] | srv | Pointer to the server that will take on the attributes. |
[in] | securityAttributes | A list of security objects as detailed in slnetsock.h. |
| beginSecurely | Whether to activate security right away or not. This is typically set to true. |
§ HTTPServer_create()
Create an HTTPServer instance.
- Parameters
-
[in] | urlh | Array of URLHandler setup descriptors |
| numURLh | Number of elements in the urlh array |
[in] | params | Optional parameters to specify characteristics - use NULL for defaults |
- Precondition
As
with all HTTPServer API's, HTTPServer_init() must have previously been called.
- Return values
-
HTTPServer | instance handle |
NULL | if unable to create the instance |
- See also
- HTTPServer_Params_init()
-
HTTPServer_delete()
§ HTTPServer_delete()
Delete an HTTPServer instance.
- Parameters
-
[in,out] | srv | Pointer containing a handle to the instance to delete. |
- Precondition
As
with all HTTPServer API's, HTTPServer_init() must have previously been called.
§ HTTPServer_sendSimpleResponse()
void HTTPServer_sendSimpleResponse |
( |
int |
s, |
|
|
int |
status, |
|
|
const char * |
type, |
|
|
size_t |
len, |
|
|
const void * |
buf |
|
) |
| |
Send a simple, complete response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
[in] | s | TCP/IP socket connected to a client |
[in] | status | Status Code associated with the response |
[in] | type | Content-type of the response |
[in] | len | Number of bytes in the response buffer buf |
[in] | buf | Response buffer |
- Precondition
As
with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendErrorResponse()
-
HTTPServer_sendResponseChunked()
§ HTTPServer_sendResponse()
void HTTPServer_sendResponse |
( |
int |
s, |
|
|
int |
status, |
|
|
const char * |
headers[], |
|
|
int |
numHeaders, |
|
|
size_t |
len, |
|
|
const void * |
buf |
|
) |
| |
Send a complete response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
[in] | s | TCP/IP socket connected to a client |
[in] | status | Status Code associated with the response |
[in] | headers | Optional response headers |
[in] | numHeaders | number of elements in headers |
[in] | len | Number of bytes in the response buffer buf |
[in] | buf | Response buffer |
- Precondition
As
with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendErrorResponse()
-
HTTPServer_sendResponseChunked()
§ HTTPServer_sendErrorResponse()
void HTTPServer_sendErrorResponse |
( |
int |
s, |
|
|
int |
status |
|
) |
| |
Send an error response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
[in] | s | TCP/IP socket connected to a client |
[in] | status | Status Code associated with the response |
- Precondition
As
with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendResponse()
§ HTTPServer_sendResponseChunked()
void HTTPServer_sendResponseChunked |
( |
int |
s, |
|
|
int |
status, |
|
|
const char * |
type |
|
) |
| |
Begin the process of sending a chunked response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
[in] | s | TCP/IP socket connected to a client |
[in] | status | Status Code associated with the response |
[in] | type | Content-type of the response |
- Precondition
As
with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendChunk()
§ HTTPServer_sendChunk()
void HTTPServer_sendChunk |
( |
int |
s, |
|
|
const void * |
buf, |
|
|
size_t |
len |
|
) |
| |
Continue and complete the process of sending a chunked response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
[in] | s | TCP/IP socket connected to a client |
[in] | buf | Response buffer |
[in] | len | Number of bytes in the response buffer buf |
- Precondition
As
with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendChunkedResponse()
§ HTTPServer_serveSelect()
int HTTPServer_serveSelect |
( |
HTTPServer_Handle |
srv, |
|
|
const struct sockaddr * |
addr, |
|
|
int |
len, |
|
|
int |
backlog |
|
) |
| |
Begin the HTTP Server's main processing loop.
- Parameters
-
[in] | srv | Handle to the server |
[in] | addr | Address information for server startup |
[in] | len | Length of the address information structure |
[in] | backlog | Maximum number of pending connections to server |
- Return values
-
0 | Server received stop command |
-1 | Server shutdown unexpectedly |
<-1 | See HTTPServer_E error codes |
§ HTTPServer_stop()
Stop a currently running server.
In order to stop the server using this function, this must be called from an outside thread.
- Parameters
-
[in] | srv | Handle to the server being stopped |
| timeout | The time in which the server is expected to halt |
§ HTTPServer_isSessionSecure()